imx6q MII RGMII

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

imx6q MII RGMII

2,774件の閲覧回数
eliaz
Contributor II

Can the imx6q use RGMII & MII peripheries  in the same time (Can these peripheries be active in the same time)?

ラベル(2)
0 件の賞賛
返信
4 返答(返信)

2,555件の閲覧回数
eliaz
Contributor II

can you be more specific about multiplexing , which signal is shared between the interfaces?

0 件の賞賛
返信

2,555件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

 

 IMX6Q has ENET module, which supports MII, RMII, RGMII interfaces

Pins affected are described in Table 23-1 (ENET External Signals) of

the i.MX6 RM (Rev. 3, 07/2015). Only single interface may be used

at a time because of multiplexing. 

 

Have a great day,

Yuri

 

------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct

Answer button. Thank you!

------------------------------------------------------------------------------

0 件の賞賛
返信

2,555件の閲覧回数
eliaz
Contributor II

can you be more specific about multiplexing , which signal is shared between the interfaces?

0 件の賞賛
返信

2,555件の閲覧回数
eliaz
Contributor II

can you be more specific about multiplexing , which signal is shared between the interfaces?

0 件の賞賛
返信