imx6q: Get the kernel source code for L3.10.17_1.0.0_IMX6DQLS_BUNDLE

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

imx6q: Get the kernel source code for L3.10.17_1.0.0_IMX6DQLS_BUNDLE

1,157件の閲覧回数
pj0585
Contributor III

Hello,

How do I get the linux kernel source code for the imx6q sabre-sd board corresponding to the "L3.10.17_1.0.0_IMX6DQLS_BUNDLE" release?

I do not want to build the entire yocto project just for getting the kernel. Any git link from which I can download the kernel source?

-Pj

ラベル(3)
0 件の賞賛
返信
2 返答(返信)

904件の閲覧回数
fabio_estevam
NXP Employee
NXP Employee
0 件の賞賛
返信

904件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Prasant

please look below discussion for git links

Re: difference between Yocto Community BSP and Freescale BSP Release

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信