imx6q: Get the kernel source code for L3.10.17_1.0.0_IMX6DQLS_BUNDLE

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

imx6q: Get the kernel source code for L3.10.17_1.0.0_IMX6DQLS_BUNDLE

797 次查看
pj0585
Contributor III

Hello,

How do I get the linux kernel source code for the imx6q sabre-sd board corresponding to the "L3.10.17_1.0.0_IMX6DQLS_BUNDLE" release?

I do not want to build the entire yocto project just for getting the kernel. Any git link from which I can download the kernel source?

-Pj

标签 (3)
0 项奖励
回复
2 回复数

544 次查看
fabio_estevam
NXP Employee
NXP Employee
0 项奖励
回复

544 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Prasant

please look below discussion for git links

Re: difference between Yocto Community BSP and Freescale BSP Release

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复