imx6q: Get the kernel source code for L3.10.17_1.0.0_IMX6DQLS_BUNDLE

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx6q: Get the kernel source code for L3.10.17_1.0.0_IMX6DQLS_BUNDLE

818 Views
pj0585
Contributor III

Hello,

How do I get the linux kernel source code for the imx6q sabre-sd board corresponding to the "L3.10.17_1.0.0_IMX6DQLS_BUNDLE" release?

I do not want to build the entire yocto project just for getting the kernel. Any git link from which I can download the kernel source?

-Pj

Labels (3)
0 Kudos
Reply
2 Replies

565 Views
fabio_estevam
NXP Employee
NXP Employee
0 Kudos
Reply

565 Views
igorpadykov
NXP Employee
NXP Employee

Hi Prasant

please look below discussion for git links

Re: difference between Yocto Community BSP and Freescale BSP Release

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply