imx6q: Android: List of sensors/devices supported by aosp

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx6q: Android: List of sensors/devices supported by aosp

1,274 Views
pj0585
Contributor III

Hi,

We are planning a custom board based on imx6q and we are planning to use android.

We want to use sensors/devices like : IMU, NFC, Temperature sensors etc.

Is there a list of supported sensors/devices published by google that have linux driver + Android HAL code already available in AOSP (8.1+) ? The intent is to use our parts from our previous projects (not android) without putting drivers /HAL development effort for the new android project.

Can somebody please point me to such a list?

Any inputs on the above will be of help.

Thanks & regards, Pj

Labels (3)
Tags (2)
0 Kudos
Reply
1 Reply

1,167 Views
b36401
NXP Employee
NXP Employee

Our Android BSP supports our i.MX boards: EVK and SABRE ones.
You can refer Android Release Notes from documentation bundle.

0 Kudos
Reply