imx6q: Android: List of sensors/devices supported by aosp

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

imx6q: Android: List of sensors/devices supported by aosp

1,234件の閲覧回数
pj0585
Contributor III

Hi,

We are planning a custom board based on imx6q and we are planning to use android.

We want to use sensors/devices like : IMU, NFC, Temperature sensors etc.

Is there a list of supported sensors/devices published by google that have linux driver + Android HAL code already available in AOSP (8.1+) ? The intent is to use our parts from our previous projects (not android) without putting drivers /HAL development effort for the new android project.

Can somebody please point me to such a list?

Any inputs on the above will be of help.

Thanks & regards, Pj

ラベル(3)
タグ(2)
0 件の賞賛
返信
1 返信

1,127件の閲覧回数
b36401
NXP Employee
NXP Employee

Our Android BSP supports our i.MX boards: EVK and SABRE ones.
You can refer Android Release Notes from documentation bundle.

0 件の賞賛
返信