imx6dl ddr 从DRAM_D16 开始

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

imx6dl ddr 从DRAM_D16 开始

680 次查看
jiaxingliang
Contributor I

由于某种原因,DDR的data只能从DRAM_D16开始到DRAM_D31

请问怎么用I.MX6DQSDL DDR3 Script Aid V0.10 配置这样子的inc文件

 

//=============================================================================			
//init script for i.Mx6DL DDR3			
//=============================================================================			
// Revision History			
// v01			
//=============================================================================			
			
wait = on			
//=============================================================================			
// Disable	WDOG		
//=============================================================================			
//setmem /16	0x020bc000 =	0x30	
			
//=============================================================================			
// Enable all clocks (they are disabled by ROM code)			
//=============================================================================			
setmem /32	0x020c4068 =	0xffffffff	
setmem /32	0x020c406c =	0xffffffff	
setmem /32	0x020c4070 =	0xffffffff	
setmem /32	0x020c4074 =	0xffffffff	
setmem /32	0x020c4078 =	0xffffffff	
setmem /32	0x020c407c =	0xffffffff	
setmem /32	0x020c4080 =	0xffffffff	
setmem /32	0x020c4084 =	0xffffffff	
			
//=============================================================================			
// IOMUX			
//=============================================================================			
//DDR IO TYPE:			
setmem /32	0x020e0774 =	0x000C0000	// IOMUXC_SW_PAD_CTL_GRP_DDR_TYPE 
setmem /32	0x020e0754 =	0x00000000	// IOMUXC_SW_PAD_CTL_GRP_DDRPKE 
			
//CLOCK:			
setmem /32	0x020e04ac =	0x00000030	// IOMUXC_SW_PAD_CTL_PAD_DRAM_SDCLK_0
setmem /32	0x020e04b0 =	0x00000030	// IOMUXC_SW_PAD_CTL_PAD_DRAM_SDCLK_1
			
//ADDRESS:			
setmem /32	0x020e0464 =	0x00000030	// IOMUXC_SW_PAD_CTL_PAD_DRAM_CAS
setmem /32	0x020e0490 =	0x00000030	// IOMUXC_SW_PAD_CTL_PAD_DRAM_RAS
setmem /32	0x020e074c =	0x00000030	// IOMUXC_SW_PAD_CTL_GRP_ADDDS 
			
//Control:			
setmem /32	0x020e0494 =	0x00000030	// IOMUXC_SW_PAD_CTL_PAD_DRAM_RESET
setmem /32	0x020e04a0 =	0x00000000	// IOMUXC_SW_PAD_CTL_PAD_DRAM_SDBA2 - DSE can be configured using Group Control Register: IOMUXC_SW_PAD_CTL_GRP_CTLDS
setmem /32	0x020e04b4 =	0x00000030	// IOMUXC_SW_PAD_CTL_PAD_DRAM_SDODT0
setmem /32	0x020e04b8 =	0x00000030	// IOMUXC_SW_PAD_CTL_PAD_DRAM_SDODT1
setmem /32	0x020e076c =	0x00000030	// IOMUXC_SW_PAD_CTL_GRP_CTLDS 
			
//Data Strobes:			
setmem /32	0x020e0750 =	0x00020000	// IOMUXC_SW_PAD_CTL_GRP_DDRMODE_CTL 
//setmem /32	0x020e04bc =	0x00000030	// IOMUXC_SW_PAD_CTL_PAD_DRAM_SDQS0 
//setmem /32	0x020e04c0 =	0x00000030	// IOMUXC_SW_PAD_CTL_PAD_DRAM_SDQS1 
setmem /32	0x020e04c4 =	0x00000030	// IOMUXC_SW_PAD_CTL_PAD_DRAM_SDQS2 
setmem /32	0x020e04c8 =	0x00000030	// IOMUXC_SW_PAD_CTL_PAD_DRAM_SDQS3 
//setmem /32	0x020e04cc =	0x00000030	// IOMUXC_SW_PAD_CTL_PAD_DRAM_SDQS4 
//setmem /32	0x020e04d0 =	0x00000030	// IOMUXC_SW_PAD_CTL_PAD_DRAM_SDQS5 
//setmem /32	0x020e04d4 =	0x00000030	// IOMUXC_SW_PAD_CTL_PAD_DRAM_SDQS6 
//setmem /32	0x020e04d8 =	0x00000030	// IOMUXC_SW_PAD_CTL_PAD_DRAM_SDQS7 
			
//Data:			
setmem /32	0x020e0760 =	0x00020000	// IOMUXC_SW_PAD_CTL_GRP_DDRMODE
//setmem /32	0x020e0764 =	0x00000030	// IOMUXC_SW_PAD_CTL_GRP_B0DS 
//setmem /32	0x020e0770 =	0x00000030	// IOMUXC_SW_PAD_CTL_GRP_B1DS 
setmem /32	0x020e0778 =	0x00000030	// IOMUXC_SW_PAD_CTL_GRP_B2DS 
setmem /32	0x020e077c =	0x00000030	// IOMUXC_SW_PAD_CTL_GRP_B3DS 
//setmem /32	0x020e0780 =	0x00000030	// IOMUXC_SW_PAD_CTL_GRP_B4DS 
//setmem /32	0x020e0784 =	0x00000030	// IOMUXC_SW_PAD_CTL_GRP_B5DS 
//setmem /32	0x020e078c =	0x00000030	// IOMUXC_SW_PAD_CTL_GRP_B6DS 
//setmem /32	0x020e0748 =	0x00000030	// IOMUXC_SW_PAD_CTL_GRP_B7DS 
			
//setmem /32	0x020e0470 =	0x00000030	// IOMUXC_SW_PAD_CTL_PAD_DRAM_DQM0
//setmem /32	0x020e0474 =	0x00000030	// IOMUXC_SW_PAD_CTL_PAD_DRAM_DQM1
setmem /32	0x020e0478 =	0x00000030	// IOMUXC_SW_PAD_CTL_PAD_DRAM_DQM2
setmem /32	0x020e047c =	0x00000030	// IOMUXC_SW_PAD_CTL_PAD_DRAM_DQM3
//setmem /32	0x020e0480 =	0x00000030	// IOMUXC_SW_PAD_CTL_PAD_DRAM_DQM4
//setmem /32	0x020e0484 =	0x00000030	// IOMUXC_SW_PAD_CTL_PAD_DRAM_DQM5
//setmem /32	0x020e0488 =	0x00000030	// IOMUXC_SW_PAD_CTL_PAD_DRAM_DQM6
//setmem /32	0x020e048c =	0x00000030	// IOMUXC_SW_PAD_CTL_PAD_DRAM_DQM7
			
			
//=============================================================================			
// DDR Controller Registers			
//=============================================================================			
// Manufacturer:	Hynix		
// Device Part Number:	H5TQ2G63GFR-RDC		
// Clock Freq.: 	400MHz		
// Density per CS in Gb: 	2		
// Chip Selects used:	1		
// Number of Banks:	8		
// Row address:    	14		
// Column address: 	10		
// Data bus width	16		
//=============================================================================			
setmem /32	0x021b001c =	0x00008000	MMDC0_MDSCR, set the Configuration request bit during MMDC set up
			
//=============================================================================			
// Calibration setup.			
//=============================================================================			
setmem /32	0x021b0800 =	0xA1390003	// DDR_PHY_P0_MPZQHWCTRL, enable both one-time & periodic HW ZQ calibration.
			
// For target board, may need to run write leveling calibration to fine tune these settings.			
//setmem /32	0x021b080c  =	0x00000000	
setmem /32	0x021b0810 =	0x00000000	
//setmem /32	0x021b480c  =	0x00000000	
//setmem /32	0x021b4810 =	0x00000000	
			
////Read DQS Gating calibration			
//setmem /32	0x021b083c =	0x00000000	// MPDGCTRL0 PHY0
setmem /32	0x021b0840 =	0x00000000	// MPDGCTRL1 PHY0
//setmem /32	0x021b483c =	0x00000000	// MPDGCTRL0 PHY1
//setmem /32	0x021b4840 =	0x00000000	// MPDGCTRL1 PHY1
			
//Read calibration			
//setmem /32	0x021b0848 =	0x40404040	// MPRDDLCTL PHY0
setmem /32	0x021b4848 =	0x40404040	// MPRDDLCTL PHY1
			
//Write calibration                     			
//setmem /32	0x021b0850 =	0x40404040	// MPWRDLCTL PHY0
setmem /32	0x021b4850 =	0x40404040	// MPWRDLCTL PHY1
			
//read data bit delay: (3 is the reccommended default value, although out of reset value is 0)			
//setmem /32	0x021b081c =	0x33333333	// DDR_PHY_P0_MPREDQBY0DL3
//setmem /32	0x021b0820 =	0x33333333	// DDR_PHY_P0_MPREDQBY1DL3
setmem /32	0x021b0824 =	0x33333333	// DDR_PHY_P0_MPREDQBY2DL3
setmem /32	0x021b0828 =	0x33333333	// DDR_PHY_P0_MPREDQBY3DL3
//setmem /32	0x021b481c =	0x33333333	// DDR_PHY_P1_MPREDQBY0DL3
//setmem /32	0x021b4820 =	0x33333333	// DDR_PHY_P1_MPREDQBY1DL3
//setmem /32	0x021b4824 =	0x33333333	// DDR_PHY_P1_MPREDQBY2DL3
//setmem /32	0x021b4828 =	0x33333333	// DDR_PHY_P1_MPREDQBY3DL3
			
//For i.mx6qd parts of versions A & B (v1.0, v1.1), uncomment the following lines. For version C (v1.2), keep commented			
//setmem /32	0x021b08c0 =	0x24911492	// fine tune SDCLK duty cyc to low - seen to improve measured duty cycle of i.mx6
//setmem /32	0x021b48c0 =	0x24911492	
			
// Complete calibration by forced measurement:                  			
//setmem /32	0x021b08b8 = 	0x00000800	// DDR_PHY_P0_MPMUR0, frc_msr
setmem /32	0x021b48b8 = 	0x00000800	// DDR_PHY_P0_MPMUR0, frc_msr
//=============================================================================			
// Calibration setup end			
//=============================================================================			
			
//MMDC init: 			
setmem /32	0x021b0004 =	0x0002002D	// MMDC0_MDPDC
setmem /32	0x021b0008 =	0x00333040	// MMDC0_MDOTC
setmem /32	0x021b000c =	0x3F4352F3	// MMDC0_MDCFG0
setmem /32	0x021b0010 =	0xB66D8B63	// MMDC0_MDCFG1
setmem /32	0x021b0014 =	0x01FF00DB	// MMDC0_MDCFG2
			
//MDMISC: RALAT kept to the high level of 5. 			
//MDMISC: consider reducing RALAT if your 528MHz board design allow that. Lower RALAT benefits: 			
//a. better operation at low frequency, for LPDDR2 freq < 100MHz, change RALAT to 3			
//b. Small performence improvment 			
setmem /32	0x021b0018 =	0x00011740	// MMDC0_MDMISC
setmem /32	0x021b001c =	0x00008000	// MMDC0_MDSCR, set the Configuration request bit during MMDC set up
setmem /32	0x021b002c =	0x000026D2	// MMDC0_MDRWD
setmem /32	0x021b0030 =	0x00431023	// MMDC0_MDOR
setmem /32	0x021b0040 =	0x0000000F	// Chan0 CS0_END 
setmem /32	0x021b0000 =	0x83180000	// MMDC0_MDCTL
			
//Mode register writes                 			
setmem /32	0x021b001c =	0x02008032	// MMDC0_MDSCR, MR2 write, CS0
setmem /32	0x021b001c =	0x00008033	// MMDC0_MDSCR, MR3 write, CS0
setmem /32	0x021b001c =	0x00048031	// MMDC0_MDSCR, MR1 write, CS0
setmem /32	0x021b001c =	0x15208030	// MMDC0_MDSCR, MR0write, CS0
setmem /32	0x021b001c =	0x04008040	// MMDC0_MDSCR, ZQ calibration command sent to device on CS0
			
//setmem /32	0x021b001c =	0x0200803A	// MMDC0_MDSCR, MR2 write, CS1
//setmem /32	0x021b001c =	0x0000803B	// MMDC0_MDSCR, MR3 write, CS1
//setmem /32	0x021b001c =	0x00048039	// MMDC0_MDSCR, MR1 write, CS1
//setmem /32	0x021b001c =	0x15208038	// MMDC0_MDSCR, MR0write, CS1
//setmem /32	0x021b001c =	0x04008048	// MMDC0_MDSCR, ZQ calibration command sent to device on CS1
			
setmem /32	0x021b0020 =	0x00007800	// MMDC0_MDREF
			
setmem /32	0x021b0818 =	0x00022227	// DDR_PHY_P0_MPODTCTRL
setmem /32	0x021b4818 =	0x00022227	// DDR_PHY_P1_MPODTCTRL
			
setmem /32	0x021b0004 =	0x0002556D	// MMDC0_MDPDC now SDCTL power down enabled
			
setmem /32	0x021b0404 =	0x00011006	// MMDC0_MAPSR ADOPT power down enabled, MMDC will enter automatically to self-refresh while the number of idle cycle reached.
			
setmem /32	0x021b001c =	0x00000000	// MMDC0_MDSCR, clear this register (especially the configuration bit as initialization is complete)
			
		
			

 

DDR-faild.pngDDR.png

0 项奖励
回复
1 回复

639 次查看
Dhruvit
NXP TechSupport
NXP TechSupport
 
I hope you are doing well
 
To access the particular DDR block, one needs to use chip select.
Please refer to section 44.4.4.2 Chip select settings from the Reference Manual IMX6DQRM.
Please configure the registers accordingly.
 
I hope this information helps you.
 
Thanks & Regards
Sanket Parekh
0 项奖励
回复