imx6dl-Android lollipop Ethernet issue

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

imx6dl-Android lollipop Ethernet issue

1,122 次查看
小樺陳
Contributor I

my os: android 5.0

platform:imx6dl

It happened when i download default source code

When i ping to www.google.com

it will fail

my setting as below

ping 210.242.127.54 ==>0K (host:www.google.com)

ping www.google.com==>fail

#getprop | grep

dhcp.eth1.dns1:10.1.0.19

dhcp.eth1.dns2:10.1.0.17

0 项奖励
回复
1 回复

955 次查看
b36401
NXP Employee
NXP Employee

Possibly the board has no route to the network your DNS servers 10.1.0.17 and 10.1.0.19 are located in.

So the system fails to resolve www.google.com name into 210.242.127.54 IP.

Please try to set 8.8.8.8 DNS server instead.

Have a great day,

Victor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复