imx6dl-Android lollipop Ethernet issue

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx6dl-Android lollipop Ethernet issue

1,118 Views
小樺陳
Contributor I

my os: android 5.0

platform:imx6dl

It happened when i download default source code

When i ping to www.google.com

it will fail

my setting as below

ping 210.242.127.54 ==>0K (host:www.google.com)

ping www.google.com==>fail

#getprop | grep

dhcp.eth1.dns1:10.1.0.19

dhcp.eth1.dns2:10.1.0.17

0 Kudos
Reply
1 Reply

951 Views
b36401
NXP Employee
NXP Employee

Possibly the board has no route to the network your DNS servers 10.1.0.17 and 10.1.0.19 are located in.

So the system fails to resolve www.google.com name into 210.242.127.54 IP.

Please try to set 8.8.8.8 DNS server instead.

Have a great day,

Victor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply