imx6UL SOM with full External Interface Module EIM?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

imx6UL SOM with full External Interface Module EIM?

1,678件の閲覧回数
alf_rieckmann
Contributor I

Would anybody know of an imx6UL based SoM with the complete External Interface Module Bus EIM brought to pins?

We would like to connect an FPGA to it (SRAM mode).

Other requirements for the SoM: (low cost, low power)

Format: SoDIMM or any other will work.

No Wireless, no LCD or display, no camera.

Flash: QSPI or eMMC (and not parallel-NAND).

T100 PHY or RMII pins.

1 USB, 1 UART, 1 SPI, 1 I2C.

ラベル(2)
0 件の賞賛
返信
1 返信

1,605件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi alf rieckmann

one can look at

The OPOS6UL board: a very competitive embedded Linux board 

Index of /_downloads/opos6ul/documentation 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信