imx6UL SOM with full External Interface Module EIM?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

imx6UL SOM with full External Interface Module EIM?

1,243 次查看
alf_rieckmann
Contributor I

Would anybody know of an imx6UL based SoM with the complete External Interface Module Bus EIM brought to pins?

We would like to connect an FPGA to it (SRAM mode).

Other requirements for the SoM: (low cost, low power)

Format: SoDIMM or any other will work.

No Wireless, no LCD or display, no camera.

Flash: QSPI or eMMC (and not parallel-NAND).

T100 PHY or RMII pins.

1 USB, 1 UART, 1 SPI, 1 I2C.

标签 (2)
0 项奖励
回复
1 回复

1,170 次查看
igorpadykov
NXP Employee
NXP Employee

Hi alf rieckmann

one can look at

The OPOS6UL board: a very competitive embedded Linux board 

Index of /_downloads/opos6ul/documentation 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复