imx6 using adv7180 to crop input image size

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

imx6 using adv7180 to crop input image size

1,135 次查看
loujenwei
Contributor I

I am  use SABRE Automotive board, and BSP is  L3.0.35_4.1.0.

use /unit_tests/mxc_v4l2_overlay.out -iw 720 -ih 480 -it 13 -ow 800 -oh 480 -fg is work fine.

but when I want to crop input image to any size -iw 320 -ih 240, and the screen is scrolling .

can I crop input image to any size ?

标签 (2)
0 项奖励
回复
1 回复

917 次查看
joanxie
NXP TechSupport
NXP TechSupport

did you try to use mxc_v4l2_tvin.out? the same issue? you can try to use gstreamer, which can support any input size if you want.

0 项奖励
回复