imx6 using adv7180 to crop input image size

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx6 using adv7180 to crop input image size

1,163 Views
loujenwei
Contributor I

I am  use SABRE Automotive board, and BSP is  L3.0.35_4.1.0.

use /unit_tests/mxc_v4l2_overlay.out -iw 720 -ih 480 -it 13 -ow 800 -oh 480 -fg is work fine.

but when I want to crop input image to any size -iw 320 -ih 240, and the screen is scrolling .

can I crop input image to any size ?

Labels (2)
0 Kudos
Reply
1 Reply

945 Views
joanxie
NXP TechSupport
NXP TechSupport

did you try to use mxc_v4l2_tvin.out? the same issue? you can try to use gstreamer, which can support any input size if you want.

0 Kudos
Reply