imx6.ulz

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx6.ulz

Jump to solution
3,004 Views
christopheferra
Contributor I

Hi,

I want to evaluate imx6.ulz. As i can understand, i should use imx6.ull evaluation board.

In the migration guide for imx6.ulz, it is written that i shoud use Linux_ 4.14.62_1.0.0 BSP.

There is an new version of the BSP : L4.14.78_1.0.0_MX6UL7D, may y use this one ?

Do you plan a imx6.ulz evaluation board ?

Sincerly,

Christophe

Labels (2)
Tags (1)
0 Kudos
Reply
1 Solution
2,830 Views
CarlosCasillas
NXP Employee
NXP Employee

Hi Christophe,

Until now, there are no plans of releasing a different evaluation board for i.MX6ULZ specific. It is supported on i.MX6ULL base board, just replacing the CPU board with the one of i.MX6ULZ processor.

Regarding software and porting guide, this document mentions the mayor considerations when migrating, so, as general guidelines, they should work with newer BSP releases, just considering the changes between BSP versions.


Hope this will be useful for you.
Best regards!
/Carlos
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

-------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
3 Replies
2,831 Views
CarlosCasillas
NXP Employee
NXP Employee

Hi Christophe,

Until now, there are no plans of releasing a different evaluation board for i.MX6ULZ specific. It is supported on i.MX6ULL base board, just replacing the CPU board with the one of i.MX6ULZ processor.

Regarding software and porting guide, this document mentions the mayor considerations when migrating, so, as general guidelines, they should work with newer BSP releases, just considering the changes between BSP versions.


Hope this will be useful for you.
Best regards!
/Carlos
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

-------------------------------------------------------------------------------

0 Kudos
Reply
2,829 Views
CarlosCasillas
NXP Employee
NXP Employee

Hi Christophe,

Have you checked AN12264?

https://www.nxp.com/docs/en/nxp/application-notes/AN12264.pdf 

Hope this will be useful for you.
Best regards!
/Carlos
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

-------------------------------------------------------------------------------

0 Kudos
Reply
2,829 Views
christopheferra
Contributor I

Hi Carlos,

I have already read the migration guide.

Thanks for your reply, i will try first the iMX6.ull.

Sincerly,

Christophe

0 Kudos
Reply