imx6.ulz

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
3,005件の閲覧回数
christopheferra
Contributor I

Hi,

I want to evaluate imx6.ulz. As i can understand, i should use imx6.ull evaluation board.

In the migration guide for imx6.ulz, it is written that i shoud use Linux_ 4.14.62_1.0.0 BSP.

There is an new version of the BSP : L4.14.78_1.0.0_MX6UL7D, may y use this one ?

Do you plan a imx6.ulz evaluation board ?

Sincerly,

Christophe

ラベル(2)
タグ(1)
0 件の賞賛
返信
1 解決策
2,831件の閲覧回数
CarlosCasillas
NXP Employee
NXP Employee

Hi Christophe,

Until now, there are no plans of releasing a different evaluation board for i.MX6ULZ specific. It is supported on i.MX6ULL base board, just replacing the CPU board with the one of i.MX6ULZ processor.

Regarding software and porting guide, this document mentions the mayor considerations when migrating, so, as general guidelines, they should work with newer BSP releases, just considering the changes between BSP versions.


Hope this will be useful for you.
Best regards!
/Carlos
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

-------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
2,832件の閲覧回数
CarlosCasillas
NXP Employee
NXP Employee

Hi Christophe,

Until now, there are no plans of releasing a different evaluation board for i.MX6ULZ specific. It is supported on i.MX6ULL base board, just replacing the CPU board with the one of i.MX6ULZ processor.

Regarding software and porting guide, this document mentions the mayor considerations when migrating, so, as general guidelines, they should work with newer BSP releases, just considering the changes between BSP versions.


Hope this will be useful for you.
Best regards!
/Carlos
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

-------------------------------------------------------------------------------

0 件の賞賛
返信
2,830件の閲覧回数
CarlosCasillas
NXP Employee
NXP Employee

Hi Christophe,

Have you checked AN12264?

https://www.nxp.com/docs/en/nxp/application-notes/AN12264.pdf 

Hope this will be useful for you.
Best regards!
/Carlos
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

-------------------------------------------------------------------------------

0 件の賞賛
返信
2,830件の閲覧回数
christopheferra
Contributor I

Hi Carlos,

I have already read the migration guide.

Thanks for your reply, i will try first the iMX6.ull.

Sincerly,

Christophe

0 件の賞賛
返信