imx6 system wake up

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

imx6 system wake up

1,594件の閲覧回数
RobertCorrellus
Contributor II

Looking for information on how to run imx6solo light in low power mode and deep sleep for 1/2 my processing time.

I can command my custom board into deep sleep mode (refer to AN4580) but have not set-up a wake up time.  I am looking for instructions on how to set up the wake time after I command the power state to "mem"?

Also looking to run very low power, with 1 G of LP DDR2  my board is pulling about 33 mA of the 56 mA total load.  Any suggestions on reducing the memory power consumption?

ラベル(2)
0 件の賞賛
返信
1 返信

1,401件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

HI Robert

I think one can look at unit tests mxc_rtc test (wake-up after some time)

Index of /buildsources/i/imx-test/imx-test-3.10.53-1.1.0

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信