gcc-4.6.2 on I.mx28

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

gcc-4.6.2 on I.mx28

1,516 次查看
jeanletutour
Contributor II

For some application gcc-4.4.4 is no more sufficient

does somebody knows how  to get this compiler gcc-4.6.2,  working for I.mx28 ?

can we compile only the application without recompiling the kernel,  and libs  ?

Thanks

标签 (2)
0 项奖励
回复
2 回复数

1,361 次查看
b36401
NXP Employee
NXP Employee

Actually it does not matter which compiler is used to compile your binaries.

However you need to make sure that you are using right libc.

Have a great day,

Victor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

1,361 次查看
jeanletutour
Contributor II

Hi Victor , and thanks for your answer , so any version of compiler may work , if you have the good libc .

does  somebody knows  where to get gcc-4.6.2-glibc-2.13-linaro-multilib-2011.12-1.i386.rpm that seems to  be the right version mentionned  in LTIB 

best regards

0 项奖励
回复