imx6 system wake up

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx6 system wake up

1,593 Views
RobertCorrellus
Contributor II

Looking for information on how to run imx6solo light in low power mode and deep sleep for 1/2 my processing time.

I can command my custom board into deep sleep mode (refer to AN4580) but have not set-up a wake up time.  I am looking for instructions on how to set up the wake time after I command the power state to "mem"?

Also looking to run very low power, with 1 G of LP DDR2  my board is pulling about 33 mA of the 56 mA total load.  Any suggestions on reducing the memory power consumption?

Labels (2)
0 Kudos
Reply
1 Reply

1,400 Views
igorpadykov
NXP Employee
NXP Employee

HI Robert

I think one can look at unit tests mxc_rtc test (wake-up after some time)

Index of /buildsources/i/imx-test/imx-test-3.10.53-1.1.0

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply