imx6 spi slave mode without SS signal

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

imx6 spi slave mode without SS signal

跳至解决方案
2,791 次查看
kurkinalexandr
Contributor III

Hello.

I am interested, if it is possible to use imx6 spi in slave mode with disconnected SS signal. I plane clear SSB_CTRL bit so that the data could be advanced "when the number of bits received in the shift register is
equal to (BURST LENGTH + 1)"

Do you know is it workable configuration, or SS signal is necessarily needs for slave mode.

Regards.

标记 (2)
0 项奖励
回复
1 解答
2,201 次查看
art
NXP Employee
NXP Employee

The SS signal is necessarily required even when operating in slave mode, since only the negation of the external SS signal latches the received burst (as defined by the BURST LENGTH + 1 parameter) from the shift register to the RxFIFO.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

4 回复数
2,201 次查看
andrewwozniak
Contributor II

Hello Artur,

Would you know if your SPI slave mode solution works for i.MX6 SoloX?

There are published errata which says:

ERR009535 - eCSPI: Burst completion by SS signal in slave mode is not functional - No fix scheduled

If this still applies, is there a potential workaround?

Thanks,
Andrew

0 项奖励
回复
2,201 次查看
art
NXP Employee
NXP Employee

The SS signal is still required in that case, since only the negation of the SS signal shifts the received burst (whose length is defined by the BURST LENGTH + 1 parameter) from the receiving shift register to the RxFIFO, thus, making the received data accessible for software.

Best Regards,
Artur

0 项奖励
回复
2,201 次查看
andrewwozniak
Contributor II

Perhaps I misunderstand the relationship between the ERRATA and your suggestion for burst mode. The errata says that "Burst completion by SS signal in slave mode is not functional". If this is true, is it possible to operation burst slave mode "without" SS signal?

Thanks,

Andrew

0 项奖励
回复
2,202 次查看
art
NXP Employee
NXP Employee

The SS signal is necessarily required even when operating in slave mode, since only the negation of the external SS signal latches the received burst (as defined by the BURST LENGTH + 1 parameter) from the shift register to the RxFIFO.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------