imx6 sabresd RTS

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx6 sabresd RTS

1,581 Views
berniechen
Contributor II

Excuse me, TI am335x have register MCR, which can control RTS active low or inactive high. Does imx6 have similar register ? Because I think serial driver have full function of RS232, it must have some register to control RTS low or high, thank you.

Labels (1)
0 Kudos
Reply
2 Replies

1,479 Views
igorpadykov
NXP Employee
NXP Employee

Hi Bernie

Uart is described in Chapter 64   IMX6DQRM

there is no option to control RTS low or high.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,479 Views
berniechen
Contributor II

Hi

But uart have full function, how do they implement RTS low and high?

0 Kudos
Reply