Does i.MX6 Linux BSP provide software to evaluate AR6003 access point?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Does i.MX6 Linux BSP provide software to evaluate AR6003 access point?

Jump to solution
1,997 Views
satoshishimoda
Senior Contributor I

Hi community,

We have a question about i.MX6DQ Linux BSP.

We want to confirm whether i.MX6DQ Linux BSP support Wi-Fi access point mode.

We guess the AR6003 driver for SABRE bord can work as access point mode, but don't know whether there is software to evaluate the mode.

Would you let me know the status of each Linux BSP?

(e.g. L3.0.35_4.1.0: NO, L3.10.17_1.0.0-ga & L3.10.35_1.0.0-ga: YES)

Best Regards,

Satoshi Shimoda

Tags (1)
0 Kudos
Reply
1 Solution
1,708 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi Satoshi Shimoda,

Please refer to "i.MX_6Dual6Quad_Linux_Reference_Manual.pdf" in "L3.0.35_4.1.0_130816_docs" which can be downloaded from FSL official web, its  "Chapter 40 AR6003 WiFi "  introduce it is a  standard linux wifi device.

    Wifi module of AR6003  works normally we tried before  in  i.MX6Q-SDP. You can use  comand " iwconfig " to set it work mode(iwconfig  --help can get help).

"iwconfig wlan0 mode master" to setup AP mode after your Wlan up.

refer to:

http://blog.csdn.net/goodlixueyong/article/details/6461871

iwconfig工具使用-windowsbbs126-ChinaUnix博客

Have a nice day

Best Regards

Dan

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
6 Replies
1,709 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi Satoshi Shimoda,

Please refer to "i.MX_6Dual6Quad_Linux_Reference_Manual.pdf" in "L3.0.35_4.1.0_130816_docs" which can be downloaded from FSL official web, its  "Chapter 40 AR6003 WiFi "  introduce it is a  standard linux wifi device.

    Wifi module of AR6003  works normally we tried before  in  i.MX6Q-SDP. You can use  comand " iwconfig " to set it work mode(iwconfig  --help can get help).

"iwconfig wlan0 mode master" to setup AP mode after your Wlan up.

refer to:

http://blog.csdn.net/goodlixueyong/article/details/6461871

iwconfig工具使用-windowsbbs126-ChinaUnix博客

Have a nice day

Best Regards

Dan

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply
1,708 Views
satoshishimoda
Senior Contributor I

Hi Dan Wang,

Thank you for your reply.

OK, I understood it supports Wi-Fi AP mode and how to setup the mode.

I appreciate your detail explanation.

Best Regards,

Satoshi Shimoda

0 Kudos
Reply
1,708 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi Satoshi Shimoda,

It's my pleasure and I am very glad it can help you.

Have a nice day.

Best Regards

Dan

0 Kudos
Reply
1,708 Views
satoshishimoda
Senior Contributor I

Please someone help me.

If AR6003 driver in Linus BSP does not support access point mode, we have to consider modifying the code or changing the Wi-Fi chip.

Best Regards,

Satoshi Shimoda

0 Kudos
Reply
1,708 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi Satoshi Shimoda,

About the access point mode can be supported in linux I am not sure, Let me confirm it for you. I will give you reply when I get the result.

Have a nice day

Best Regards

Dan

0 Kudos
Reply
1,708 Views
satoshishimoda
Senior Contributor I

Would you be able to help?

0 Kudos
Reply