imx6 rtc is getting reset after every power cycle

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

imx6 rtc is getting reset after every power cycle

4,086件の閲覧回数
niketsarda
Contributor II

Hi

We are using the imx6 in my development board (Reference from nitrogen6_max EVM).

While using RTC clock, it is getting reset after every power cycle.

Is there any pin configuration need to be update to prevent RTC reset on power cycle.

Also provide some register setting to keep RTC continuous ON


For power supply we have used  battery power supply (Battery voltage of 4.2V) on VIN pin.

We are not using LICELL pin to power RTC.

Thank you

NIket

ラベル(1)
0 件の賞賛
返信
8 返答(返信)

3,662件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Nlket

nitrogen6 board was developed is supported by third party boundary

devices, so issue may be posted to its support. In general one can check

processor VDD_SNVS_IN with oscilloscope, there should be no sags during

removing power. Also may be tested with nxp sabre sd reference board

Schematics (1)
"iMX6_SABRE_SDB_DESIGNFILES  : Design files"

SABRE Platform for Smart Devices|NXP 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

3,662件の閲覧回数
mrudangshelat
Contributor IV

Hi Igor,

sorry for the confusion here. We have not used development board (Reference from nitrogen6_max EVM) for RTC testing, but we have used our developed board based on i.MX6D based along with PMIC PF0100.

PF0100.JPG

Kindly suggest the solution as RTC goes OFF/reset mode.

We would like to have RTC to be ON continuously. Let me know what else you require.

Regards,

Mrudang.

0 件の賞賛
返信

3,662件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Nlket

had you checked processor VDD_SNVS_IN with oscilloscope ?

Best regards
igor

0 件の賞賛
返信

3,662件の閲覧回数
mrudangshelat
Contributor IV

Hi Igor,

We are getting 3.0V on VDD_SNVS_IN rail.

Regards,

Mrudang

0 件の賞賛
返信

3,662件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Nlket

 

this board is supported by its vendor, boundary devices, suggest to contact its

tech support. Just for test you can try with nxp sabre sd reference board.

 

Best regards
igor

0 件の賞賛
返信

3,662件の閲覧回数
mrudangshelat
Contributor IV

Hi Igor,

As I informed you we are not using Nitrogen EVK board. We are testing on our own developed board. And it is very similar with Sabre board. Only the change is as I mentioned earlier we didn't use LICELL pin to power RTC. SNVS is powered through VIN.

Let me know if you require any other details.

Regards,

Mrudang

0 件の賞賛
返信

3,662件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

"SNVS is powered through VIN"

so when board was powered off, does SNVS also powered off ?

You can test rtc with nxp linux bsps described on below link:

i.MX Software|NXP 

Best regards
igor

0 件の賞賛
返信

3,662件の閲覧回数
mrudangshelat
Contributor IV

Hi Igor,

Yes, when a board was powered off, SNVS rail is ON.

I guess we have solved the issue.

Thanks for the support.

Thanks,

Mrudang

0 件の賞賛
返信