imx6 problem with hdmi display

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx6 problem with hdmi display

Jump to solution
2,089 Views
admin
Specialist II

Hello all,

I am testing the board from Boundary Devices : Nitrogen6X

I am able to boot linux with their kernel. I tried to start a fedora-arm rootfs, and also their

LTIB 2012-08 image.

I can login with the console connector (with serial to usb).

My issue is that I have no display on the hdmi port. I used the bootargs to use hdmi.

I don't know what can be the cause of this issue.

here are some logs :

dmesg :dmesg - Pastebin.com

Xorg :http://pastebin.com/bssXw1pL

gdm/\:0-slave.log : gdm/:0-slave.log - Pastebin.com

xrandr - Pastebin.com

systemd-journal - Pastebin.com


many thanks.

Labels (3)
0 Kudos
Reply
1 Solution
1,302 Views
VladanJovanovic
NXP Employee
NXP Employee

Looking at the log HDMI does seem to be initialized. Have you tried any other resolution? Sometimes monitors do not support all resolutions or there can be some timing issue with the one you selected...

Vladan

View solution in original post

0 Kudos
Reply
1 Reply
1,303 Views
VladanJovanovic
NXP Employee
NXP Employee

Looking at the log HDMI does seem to be initialized. Have you tried any other resolution? Sometimes monitors do not support all resolutions or there can be some timing issue with the one you selected...

Vladan

0 Kudos
Reply