imx6 hdmi cable length

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

imx6 hdmi cable length

跳至解决方案
2,096 次查看
kurkinalexandr
Contributor III

Hello.

I wonder if there is any restriction for hdmi cable length.

For example we have 1280x800 resolution 60fps, so what maximum length can have our hdmi cable to support this resolution correctly.

We have imx6 quad inside cm-fx6 module.

Thanks

标签 (4)
标记 (2)
1 解答
1,979 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Fan

length is defined mainly by cable quality, so voltage at receiver end will be:

Input Differential Voltage Level >150mV (min.)

as stated in sect.4.2.5 HDMI Sink TMDS Characteristics HDMI specification.

May be useful to check AN4671 HDMI Compliance Test Specification

http://cache.freescale.com/files/32bit/doc/app_note/AN4671.pdf 


Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

1 回复
1,980 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Fan

length is defined mainly by cable quality, so voltage at receiver end will be:

Input Differential Voltage Level >150mV (min.)

as stated in sect.4.2.5 HDMI Sink TMDS Characteristics HDMI specification.

May be useful to check AN4671 HDMI Compliance Test Specification

http://cache.freescale.com/files/32bit/doc/app_note/AN4671.pdf 


Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------