imx6 hdmi cable length

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

imx6 hdmi cable length

ソリューションへジャンプ
2,111件の閲覧回数
kurkinalexandr
Contributor III

Hello.

I wonder if there is any restriction for hdmi cable length.

For example we have 1280x800 resolution 60fps, so what maximum length can have our hdmi cable to support this resolution correctly.

We have imx6 quad inside cm-fx6 module.

Thanks

ラベル(4)
タグ(2)
1 解決策
1,994件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Fan

length is defined mainly by cable quality, so voltage at receiver end will be:

Input Differential Voltage Level >150mV (min.)

as stated in sect.4.2.5 HDMI Sink TMDS Characteristics HDMI specification.

May be useful to check AN4671 HDMI Compliance Test Specification

http://cache.freescale.com/files/32bit/doc/app_note/AN4671.pdf 


Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

1 返信
1,995件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Fan

length is defined mainly by cable quality, so voltage at receiver end will be:

Input Differential Voltage Level >150mV (min.)

as stated in sect.4.2.5 HDMI Sink TMDS Characteristics HDMI specification.

May be useful to check AN4671 HDMI Compliance Test Specification

http://cache.freescale.com/files/32bit/doc/app_note/AN4671.pdf 


Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------