imx6 flashing sparse image using uuu

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

imx6 flashing sparse image using uuu

1,315件の閲覧回数
maos
Contributor I

Hi!

Working on an imx6ull based board.

We are creating a custom image in yocto where we have a rather large but empty partition (ext4 filesystem created in this partition but no data).

Downloading the resulting image takes about 10 minutes but we need to reduce this time.

So far we have used:
uuu -b emmc_all <path to u-boot> <path to .wic.bz2 file>/*

Looking at the the decompressed .wic file it is about 3.6 G but most of this should be zeros/empty space.

I think one can draw this conclusion also looking at the generated rootfs.wic.bmap-file as it states:
<!-- Image size in bytes: 3.5 GiB -->
<ImageSize> 3790602240 </ImageSize>

<!-- Size of a block in bytes -->
<BlockSize> 4096 </BlockSize>

<!-- Count of blocks in the image file -->
<BlocksCount> 925440 </BlocksCount>

<!-- Count of mapped blocks: 514.2 MiB or 14.2% -->
<MappedBlocksCount> 131631 </MappedBlocksCount>

Also tried to convert the .wic file using android's img2simg.
When trying the resulting file using the inbuild "emmc_all" script the bootloader started (booting from bootpartition?) but couldn't find a partition table.

Have also made various attempts using a custom uuu-script based on the "emmc_all" inbuilt scipt.

Is there some way to do a "sparse flashing" using uuu?
And could someone point me to how to do this?

thanks,
Mårten

 

0 件の賞賛
返信
1 返信

1,292件の閲覧回数
AldoG
NXP TechSupport
NXP TechSupport

Hello,

A couple of tips that can reduce the time of flashing would be:

- Do not use wic.bz2 use standard .wic file, since the tool will decompress first and then start flashing.
- Try build one smaller image.
- Remove message from uart port. Debug message takes some time to transfer to uart port even when it's not connected.

Best regards,
Aldo.

0 件の賞賛
返信