Hi all,
I'm trying to connect via JTAG to the MCIMX6UL-EVK with "J-link base" from Segger.
First of all i have removed R1407, R1431~R1434 because JTAG is dedicated with Audio CODEC signals. This is said in Hardware User's guide, page 14.
I have also removed R507 so the JTAG interface is configured to a mode compliant with the IEEE 1149.1 standard, (IMX6ULHDG.pdf)
So at this point, i try to connect with no success.
Please, find attached 2 screen captures. One picture with R507 placed (just in case) and another one without it.
Check this out and any help will be appreciated.
In device options, i don't see any IMX6.
Though in the screen captures is shown ARM7 as device option, i have tried with cortex-A7 with same results.
Thanks and best regards