imx6 cpu tap not found in jtag chain

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

imx6 cpu tap not found in jtag chain

ソリューションへジャンプ
6,898件の閲覧回数
alubeiro
Contributor IV

Hi all,

I'm trying to connect via JTAG to the MCIMX6UL-EVK with "J-link base" from Segger.

First of all i have removed R1407, R1431~R1434 because JTAG is dedicated with Audio CODEC signals. This is said in Hardware User's guide, page 14.

I have also removed R507 so the JTAG interface is configured to a mode compliant with the IEEE 1149.1 standard, (IMX6ULHDG.pdf)

So at this point, i try to connect with no success.

Please, find attached 2 screen captures. One picture with R507 placed (just in case) and another one without it.

Check this out and any help will be appreciated.

In device options, i don't see any IMX6.

Though in the screen captures is shown ARM7 as device option, i have tried with cortex-A7 with same results.

Thanks and best regards

ラベル(1)
0 件の賞賛
返信
1 解決策
5,340件の閲覧回数
alubeiro
Contributor IV

Hi Igor,

Finally we got it! we had removed R507 before trying with Cortex-A7,

Now our goal is to change the USB_LDO voltage by JTAG and then program the nand flash.

Is there any Aplication note or guide lines which i can follow?

I belive this post in starting to look the same as the other one i posted due to an issue with the USB.

IMX6UL USB OTG HID enumeration failure

So better we leave this here and continue in this other, are you agree?

Thanks and best regards

元の投稿で解決策を見る

0 件の賞賛
返信
5 返答(返信)
5,340件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

HI Alberto

please look at

https://community.freescale.com/docs/DOC-329192

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
5,341件の閲覧回数
dianatorres
NXP Employee
NXP Employee

Hi andreaskurrle

Please refer to this document instead:

ARM DS-5 Development Studio Debug i.MX6UL-EVK

Best regards,

Diana Torres

0 件の賞賛
返信
5,341件の閲覧回数
alubeiro
Contributor IV

Hi Igor,

I don't have the permission to get into that URL.

Could you please attach it here or send it to my mail?

Thanks and best regards

0 件の賞賛
返信
5,341件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

HI Alberto

please create service request for obtaining

these documents.

Best regards

igor

0 件の賞賛
返信
5,341件の閲覧回数
alubeiro
Contributor IV

Hi Igor,

Finally we got it! we had removed R507 before trying with Cortex-A7,

Now our goal is to change the USB_LDO voltage by JTAG and then program the nand flash.

Is there any Aplication note or guide lines which i can follow?

I belive this post in starting to look the same as the other one i posted due to an issue with the USB.

IMX6UL USB OTG HID enumeration failure

So better we leave this here and continue in this other, are you agree?

Thanks and best regards

0 件の賞賛
返信