imx6 bootup issue, endless loop

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

imx6 bootup issue, endless loop

1,686件の閲覧回数
blurencetin
Contributor II

Hi all,

 

We boot up our custom imx6 board with linux well.

But when we move to android, it failed at an endless loop.

 

We could find some i2c errors from the kernel log and camera/audio crash at android period.

It's so strange that we just used same kernel version between linux and android.

 

Anybody have tips for me?

 

Many thanks.

 

===============

Chip: imx6dl

Android: 4.3 jb1.1.0

Kernel version: 3.0.35

 

and the log as attachment.

Original Attachment has been moved to: kernel.log.zip

Original Attachment has been moved to: android.log.zip

ラベル(3)
タグ(3)
0 件の賞賛
返信
1 返信

1,477件の閲覧回数
jaymind
Contributor IV

Hello Blurence,

Its seems to be some dummy I2C device type related.

See some below links, may it help you

http://linux-i2c.vger.kernel.narkive.com/e0hiIeXZ/patch-i2c-match-dummy-devices-by-type

http://www.avrfreaks.net/forum/linux-2618-crash-i2c-twi-driver

common from above links and other search, may be you need to be patch driver, may be.

Thanks and Regards

JAYMIN D

0 件の賞賛
返信