imx6 bootloader - kernel bad CRC

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

imx6 bootloader - kernel bad CRC

ソリューションへジャンプ
11,111件の閲覧回数
xavierboucher
Contributor III

Hi,

I get stuck when the u-boot is suppose to start the kernel. It is always saying bad CRC. I tried 3 different kernels, one from ltib, one from buildroot and one from timesys. I am pretty sure there is at least one good CRC kernel. Do you have something on this that I can look onto? I am pretty clueless on this.

Thank you!

U-Boot 2014.04-rc3-00014-g04d2f0a-dirty (Apr 11 2014 - 14:19:47)

CPU:   Freescale i.MX6SOLO rev1.1 at 792 MHz
Reset cause: POR
Board: Wandboard
DRAM:  512 MiB
MMC:   MMC XAVIER:   XAVIER:   Setup sdhc 1.
XAVIER:   End setup.
FSL_SDHC: 0
MMC finished
In:    serial
Out:   serial
Err:   serial
Net:   Board Net Initialization Failed
No ethernet found.
Hit any key to stop autoboot:  0
=> fatload mmc 0 0x10008000 uImage
XAVIER:   Get mmc cd 1.
XAVIER:   RET: 1
reading uImage
2623120 bytes read in 153 ms (16.3 MiB/s)
=> bootm 0x10008000
## Booting kernel from Legacy Image at 10008000 ...
   Image Name:   Linux-3.0.35-ts-armv7l
   Image Type:   ARM Linux Kernel Image (uncompressed)
   Data Size:    2623056 Bytes = 2.5 MiB
   Load Address: 10008000
   Entry Point:  10008000
   Verifying Checksum ... Bad Data CRC
ERROR: can't get kernel image!

ラベル(1)
タグ(5)
0 件の賞賛
返信
1 解決策
8,264件の閲覧回数
xavierboucher
Contributor III

I found out the problem. It was only a missing define in the bootloader. I had to add the line:

#define BOOTZ

To have CRC correct.

Thank you Fabio for all your help!

元の投稿で解決策を見る

0 件の賞賛
返信
11 返答(返信)
8,265件の閲覧回数
fabio_estevam
NXP Employee
NXP Employee

Your kernel has a wrong loadaddr. For mx6solo you should build your kernel like:

make -j4 uImage LOADADDR=0x800080000

Regards,

Fabio Estevam

0 件の賞賛
返信
8,264件の閲覧回数
xavierboucher
Contributor III

Thank you Fabio for the quick answer.

Unfortunately, it does not seems to correct the problem. I used LOADADDR=0x80008000. Is this correct, just wondering because the address you gave me is 9bytes long instead of 8?

If this is ok, could it be a problem coming from the bootloader itself?

Here is the error with the kernel at 0x80008000. I used the last kernel in the freesclae imx6 repository. Thank you again:

U-Boot 2014.04-rc3-00014-g04d2f0a-dirty (Apr 11 2014 - 16:58:29)

CPU:   Freescale i.MX6SOLO rev1.1 at 792 MHz

Reset cause: POR

Board: Wandboard

DRAM:  512 MiB

MMC:   MMC XAVIER:   XAVIER:   Setup sdhc 1.

XAVIER:   End setup.

FSL_SDHC: 0

MMC finished

In:    serial

Out:   serial

Err:   serial

Net:   Board Net Initialization Failed

No ethernet found.

Hit any key to stop autoboot:  0

=> fatload mmc 0 10800000 uImage

XAVIER:   Get mmc cd 1.

XAVIER:   RET: 1

reading uImage

3840580 bytes read in 205 ms (17.9 MiB/s)

=> bootm 10800000

## Booting kernel from Legacy Image at 10800000 ...

   Image Name:   Linux-3.0.35-03053-g8d2b169

   Image Type:   ARM Linux Kernel Image (uncompressed)

   Data Size:    3840516 Bytes = 3.7 MiB

   Load Address: 80008000

   Entry Point:  80008000

   Verifying Checksum ... Bad Data CRC

ERROR: can't get kernel image!

=>

0 件の賞賛
返信
8,264件の閲覧回数
fabio_estevam
NXP Employee
NXP Employee

I see that you are doing

fatload mmc 0 10800000 uImage

Should be 80800000 instead.

and also:

bootm 10800000, should be 80800000 instead.

0 件の賞賛
返信
8,264件の閲覧回数
fabio_estevam
NXP Employee
NXP Employee

Oops, sorry.

The 80000000 addresses are for mx6solo-lite, not mx6solo.

So the ranges you are passing are fine.

Is this a custom board? Could be related to DDR configuration?

8,264件の閲覧回数
xavierboucher
Contributor III

It is possible it can come from the DDR configuration. We have a custom board based on the wandboard. We are using lpddr2 instead of ddr3 I checked on the u-boot config file and got this on the RAM:

#define CONFIG_SYS_MEMTEST_START    0x10000000
#define CONFIG_SYS_MEMTEST_END        (CONFIG_SYS_MEMTEST_START + 500 * SZ_1M)
#define CONFIG_LOADADDR            0x12000000
#define CONFIG_SYS_TEXT_BASE        0x17800000

As I understand, the memory range is 0x10000000 to 0x60000000 (in the wandboard solo and our board, there is 512mb RAM).

For the u-boot, I used the last u-boot in the denx repository and then configured it to use lpddr2. The wandboard is using the same configuration as the nitrogen6x for the RAM so I modified the cfg file of the nitrogen6x.

I used the lpddr2 ddr aid script v0.03 to help me. I modified the cpu clock speed to lower it to 800 and modified MMC0_MDMISC because it was S2 by default in the script but our RAM is S4.

I was able to properly start the console and I have done several write/read tests on the ram and it worked well. I also use the DDR stress test on the OTG and it passed the test without getting stuck.

Do you know where I could check to see what could be the problem?

Thank you.

Here is the final result of the lpddr2 config:

//============================================================================                   
//init script for i.Mx6S LPDDR2                   
//============================================================================                   
// Revision History                   
// v01                   
//============================================================================                   
//============================================================================                   
// Enable all clocks (they are disabled by ROM code)                   
//============================================================================   
DATA 4    0x020c8000     0x00013037    //change freq cpu to 660 mhz 0x00000037  //to 1gh 0x00000052 //800mhz 0x00000021
                
DATA 4    0x020c4068     0xffffffff           
DATA 4    0x020c406c     0xffffffff           
DATA 4    0x020c4070     0xffffffff           
DATA 4    0x020c4074     0xffffffff           
DATA 4    0x020c4078     0xffffffff           
DATA 4    0x020c407c     0xffffffff           
DATA 4    0x020c4080     0xffffffff           
DATA 4    0x020c4084     0xffffffff           

//Difference - pre_periph_clk_sel est a 10 pour eux, nous
DATA 4    0x020c4018      0x00860324     //Xavier - try to 307Mhz //DDR clk to 400MHz    // nous - 0x00060324   // test 307mhz 0x000A0324
//CCM_CACRR - arm clock

           
//============================================================================                   
// IOMUX                   
//============================================================================       
            
//DDR IO TYPE:                   
DATA 4    0x020e0774     0x00080000    // IOMUXC_SW_PAD_CTL_GRP_DDR_TYPE (LPDDR2)  // eux - 0x000C0000  (DDR3)       
DATA 4    0x020e0754     0x00000000    // IOMUXC_SW_PAD_CTL_GRP_DDRPKE     //eux - 0x00000000       
//CLOCK:                   
DATA 4    0x020e04ac     0x00000030    // IOMUXC_SW_PAD_CTL_PAD_DRAM_SDCLK_0    //eux - 0x00020030 - CMOS inout vs differential mode   
DATA 4    0x020e04b0     0x00000030    // IOMUXC_SW_PAD_CTL_PAD_DRAM_SDCLK_1    //eux - 0x00020030 - CMOS inout vs
//ADDRESS:                   
DATA 4    0x020e0464     0x00000030    // IOMUXC_SW_PAD_CTL_PAD_DRAM_CAS    //eux - 0x00020030 - CMOS inout vs   
DATA 4    0x020e0490     0x00000030    // IOMUXC_SW_PAD_CTL_PAD_DRAM_RAS    //eux - 0x00020030 - CMOS inout vs   
DATA 4    0x020e074c     0x00000030    // IOMUXC_SW_PAD_CTL_GRP_ADDDS         //eux - 0x00000030
//Control:                   
DATA 4    0x020e0494     0x00020000    // IOMUXC_SW_PAD_CTL_PAD_DRAM_RESET    //eux - 0x00020030 - CMOS inout vs // nous - 0x00000030, mettre a 0 car pin disabled donc Hi Z
DATA 4    0x020e04a0     0x00000000    // IOMUXC_SW_PAD_CTL_PAD_DRAM_SDBA2 - DSE can be configured using Group Control Register: IOMUXC_SW_PAD_CTL_GRP_CTLDS        //eux - 0x00000000
DATA 4    0x020e04b4     0x00000030    // IOMUXC_SW_PAD_CTL_PAD_DRAM_SDODT0    //eux - 0x00003030
DATA 4    0x020e04b8     0x00000030    // IOMUXC_SW_PAD_CTL_PAD_DRAM_SDODT1    //eux - 0x00003030   
DATA 4    0x020e076c     0x00000030    // IOMUXC_SW_PAD_CTL_GRP_CTLDS         //eux - 0x00000030
//Data Strobes:                   
DATA 4    0x020e0750     0x00020000    // IOMUXC_SW_PAD_CTL_GRP_DDRMODE_CTL     //eux - 0x00020000 - diff mode ici???
DATA 4    0x020e04bc     0x00003030    // IOMUXC_SW_PAD_CTL_PAD_DRAM_SDQS0     //eux - 0x00000030   
DATA 4    0x020e04c0     0x00003030    // IOMUXC_SW_PAD_CTL_PAD_DRAM_SDQS1     //eux - 0x00000030
DATA 4    0x020e04c4     0x00003030    // IOMUXC_SW_PAD_CTL_PAD_DRAM_SDQS2     //eux - 0x00000030
DATA 4    0x020e04c8     0x00003030    // IOMUXC_SW_PAD_CTL_PAD_DRAM_SDQS3     //eux - 0x00000030
//Data:                   
DATA 4    0x020e0760     0x00020000    // IOMUXC_SW_PAD_CTL_GRP_DDRMODE    //eux - 0x00020000   
DATA 4    0x020e0764     0x00000030    // IOMUXC_SW_PAD_CTL_GRP_B0DS         //eux - 0x00000030
DATA 4    0x020e0770     0x00000030    // IOMUXC_SW_PAD_CTL_GRP_B1DS         //eux - 0x00000030
DATA 4    0x020e0778     0x00000030    // IOMUXC_SW_PAD_CTL_GRP_B2DS         //eux - 0x00000030
DATA 4    0x020e077c     0x00000030    // IOMUXC_SW_PAD_CTL_GRP_B3DS         //eux - 0x00000030
DATA 4    0x020e0470     0x00000030    // IOMUXC_SW_PAD_CTL_PAD_DRAM_DQM0    //eux - 0x00020030 - CMOS inout vs
DATA 4    0x020e0474     0x00000030    // IOMUXC_SW_PAD_CTL_PAD_DRAM_DQM1    //eux - 0x00020030 - CMOS inout vs   
DATA 4    0x020e0478     0x00000030    // IOMUXC_SW_PAD_CTL_PAD_DRAM_DQM2    //eux - 0x00020030 - CMOS inout vs   
DATA 4    0x020e047c     0x00000030    // IOMUXC_SW_PAD_CTL_PAD_DRAM_DQM3    //eux - 0x00020030 - CMOS inout vs   
//============================================================================                   
// DDR Controller Registers                   
//============================================================================                   
// Manufacturer:    Micron               
// Device Part Number:    MT42L128M32D1               
// Clock Freq.:     400MHz               
// MMDC channels:     MMDC0               
// Density per CS in Gb:     4               
// Chip Selects used:    1               
// Number of Banks:    8               
// Row address:        14               
// Column address:     10               
// Data bus width    32               
//============================================================================           

       
DATA 4    0x021b001c     0x00008000    // MMDC0_MDSCR, set the Configuration request bit during MMDC set    eux - 0x00008000 up       
DATA 4    0x021b085c     0x1B4700C7    //MMDC0_MPZQLP2CTL,LPDDR2 ZQ params       
//============================================================================                   
// Calibration setup.                   
//============================================================================                   
DATA 4    0x021b0800     0xA1390000    // DDR_PHY_P0_MPZQHWCTRL, enable both one-time & periodic HW ZQ    eux - 0xA1390000 calibration.       
//ca bus abs delay                   
DATA 4    0x021b0890      0x00400000    // MMDC0_MPPDCMPR2 values of 20,40,50,60,7f tried. no difference seen    Original Values (Delete Later)    Difference?
//Read calibration                   
DATA 4    0x021b0848     0x40404040    // MPRDDLCTL PHY0       
//Write calibration                                        
DATA 4    0x021b0850     0x40404040    // MPWRDLCTL PHY0       
//dqs gating disabled (always disable for LPDDR2)                   
DATA 4    0x021b083c     0x20000000    // MMDC0_MPDGCTRL0       
DATA 4    0x021b0840     0x00000000    // MMDC0_MPDGCTRL1       
//read data bit delay: (3 is the reccommended default value, although out of reset value is 0)                   
DATA 4    0x021b081c     0x33333333    // DDR_PHY_P0_MPREDQBY0DL3    Original Values (Delete Later)    Difference?
DATA 4    0x021b0820     0x33333333    // DDR_PHY_P0_MPREDQBY1DL3    0x00009c40    0x33333333
DATA 4    0x021b0824     0x33333333    // DDR_PHY_P0_MPREDQBY2DL3    0x00000000    0x33333333
DATA 4    0x021b0828     0x33333333    // DDR_PHY_P0_MPREDQBY3DL3    0x00000000    0x33333333
//write data bit delay: (3 is the reccommended default value, although out of reset value is 0)                   
DATA 4    0x021b082c     0xF3333333    // DDR_PHY_P0_MPREDQBY0DL3    Original Values (Delete Later)    Difference?
DATA 4    0x021b0830     0xF3333333    // DDR_PHY_P0_MPREDQBY1DL3    0x00009c40    0xF3333333
DATA 4    0x021b0834     0xF3333333    // DDR_PHY_P0_MPREDQBY2DL3    0x00000000    0xF3333333
DATA 4    0x021b0838     0xF3333333    // DDR_PHY_P0_MPREDQBY3DL3    0x00000000    0xF3333333
// Complete calibration by forced measurement:                                     
DATA 4    0x021b08b8      0x00000800    // DDR_PHY_P0_MPMUR0, frc_msr       
//============================================================================                   
// Calibration setup end                   
//============================================================================                   

// Channel0 - startng address 0x80000000                   
DATA 4    0x021b0004     0x00020036    // MMDC0_MDPDC       eux - 0x0002002D
DATA 4    0x021b0008     0x00000000    // MMDC0_MDOTC         eux - 0x00333030    //Not revelant in LPDDR2
DATA 4    0x021b000c     0x33374133    // MMDC0_MDCFG0        eux - 0x40435323
DATA 4    0x021b0010     0x00100A82    // MMDC0_MDCFG1        eux - 0xB66E8D63
DATA 4    0x021b0014     0x00000093    // MMDC0_MDCFG2        eux - 0x01FF00DB
                    
//MDMISC: RALAT kept to the high level of 5.                    
//MDMISC: consider reducing RALAT if your 528MHz board design allow that. Lower RALAT benefits:                    
//a. better operation at low frequency, for LPDDR2 freq < 100MHz, change RALAT to 3                   
//b. Small performence improvment                    
DATA 4    0x021b0018     0x00001688    // MMDC0_MDMISC    0x015dc002    0x00001748  S2-S4
DATA 4    0x021b001c     0x00008000    // MMDC0_MDSCR, set the Configuration request bit during MMDC set up       
DATA 4    0x021b002c     0x0F9F26D2    // MMDC0_MDRWD        //eux - 0x000026D2
DATA 4    0x021b0030     0x00000010    // MMDC0_MDOR        //eux - 0x00431023
DATA 4    0x021b0038     0x00190778    // MMDC0_MDCFG3LP    // only LPDDR2
DATA 4    0x021b0040     0x00000017    // Chan0 CS0_END        
DATA 4    0x021b0400     0x11420000    // MMDC0_MAARCR ADOPT optimized priorities. Dyn jump disabled       
DATA 4    0x021b0000     0x83110000    // MMDC0_MDCTL       
// Channel0 : Configure DDR device:                         
//CS0                   
DATA 4    0x021b001c     0x003F8030    // MRW: BA=0 CS=0 MR_ADDR=63 MR_OP=0       
DATA 4    0x021b001c     0xFF0A8030    // MRW: BA=0 CS=0 MR_ADDR=10 MR_OP=ff       
DATA 4    0x021b001c     0x82018030    // MRW: BA=0 CS=0 MR_ADDR=1  MR_OP=c2       
DATA 4    0x021b001c     0x04028030    // MRW: BA=0 CS=0 MR_ADDR=2  MR_OP=6. tcl=8, tcwl=4       
DATA 4    0x021b001c     0x02038030    // MRW: BA=0 CS=0 MR_ADDR=3  MR_OP=2.drive=240/6       
DATA 4    0x021b0800     0xA1390003    // DDR_PHY_P0_MPZQHWCTRL, enable both one-time & periodic HW ZQ calibration.       
DATA 4    0x021b0020     0x00001800    // MMDC0_MDREF       
DATA 4    0x021b0818     0x00000000    // DDR_PHY_P0_MPODTCTRL       
DATA 4    0x021b0004     0x00025576    // MMDC0_MDPDC now SDCTL power down enabled       
DATA 4    0x021b0404     0x00011006    // MMDC0_MAPSR ADOPT power down enabled, MMDC will enter automatically to self-refresh while the number of idle cycle reached.       
DATA 4    0x021b001c     0x00000000    // MMDC0_MDSCR, clear this register (especially the configuration bit as initialization is complete)    0x01000202    0x00000000

0 件の賞賛
返信
8,264件の閲覧回数
fabio_estevam
NXP Employee
NXP Employee

Maybe you could try booting from NFS to discard some potential issue with the SD card reading that could lead to the CRC error?

0 件の賞賛
返信
8,264件の閲覧回数
xavierboucher
Contributor III

Unfortunately, we do not have an ethernet available on our board. But we have a usb OTG if it is possible to load the kernel with it. I did not find anything for the kernel (I usualy use this with u-boot).

I tried several sd cards just in case but I am still getting the same error.

Thank you.

0 件の賞賛
返信
8,265件の閲覧回数
xavierboucher
Contributor III

I found out the problem. It was only a missing define in the bootloader. I had to add the line:

#define BOOTZ

To have CRC correct.

Thank you Fabio for all your help!

0 件の賞賛
返信
8,264件の閲覧回数
mcyoyan
Contributor I

T'en ai rendu ou Xavier alors ? Oublie pas ton résumé que tu dois nous rendre a chaque jour !

Yan Gagnon

President | CEO

GG Telecom

SPYPOINT and XCEL products

Le 2014-04-14 à 16:29, Xavier Boucher <[email protected]> a écrit :

imx6 bootloader - kernel bad CRC

reply from Xavier Boucher in i.MX Community - View the full discussion

I found out the problem. It was only a missing define in the bootloader. I had to add the line:

#define BOOTZ

To have CRC correct.

Thank you Fabio for all your help!

Reply to this message by replying to this email, or go to the message on Freescale Community

Start a new discussion in i.MX Community by email or at Freescale Community

Following Xavier Boucher in these streams: Inbox

0 件の賞賛
返信
8,264件の閲覧回数
fabio_estevam
NXP Employee
NXP Employee

Do you mean?

#define CONFIG_CMD_BOOTZ

This one is used if you want to boot a zImage, which does not contain the embedded CRC.

0 件の賞賛
返信
8,264件の閲覧回数
xavierboucher
Contributor III

Yes, this is the define. I do not understand myself but since adding this, I am able to have good CRC on the linux kernel.

0 件の賞賛
返信