Hi Carson,
once enabled watchdog can not be disabled. So one needs
to rebuild sources, procedure is described in i.MX_6Dual6Quad_Linux_Reference_Manual.pdf
Chapter 43 Watchdog (WDOG) Driver :
use the ./ltib -c
command when located in the <ltib dir>. On the screen displayed, select Configure the
Kernel and exit. When the next screen appears, select the following option to enable this
module:
• CONFIG_IMX2_WDT-Enables Watchdog timer module. This option is available
under Device Drivers > Watchdog Timer Support > IMX2+ Watchdog.
or just comment function imx6q_add_imx2_wdt (board-mx6q_sabresd.c)
Otherwise seems there is no other option as to pet the dog manually. :smileywink: