imx6 auto reboot after set HDMI

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx6 auto reboot after set HDMI

Jump to solution
2,546 Views
lei_zhang1
Contributor I

My board is i.MX 6Quad SABRE-SD.

I burn android demo images(IMX_O8.0.0_1.0.0_ANDROID_DEMO_SD) with MFGTOOLS,it boots normally.

Then I set HDMI boot environment: 

U-Boot > setenv bootcmd boota mmc1
U-Boot > setenv bootargs console=ttymxc0,115200 androidboot.console=ttymxc0 consoleblank=0 vmalloc=128M init=/init video=mxcfb0:dev=hdmi,1920x1080M@60,bpp=32 video=mxcfb1:off video=mxcfb2:off video=mxcfb3:off androidboot.hardware=freescale cma=448M galcore.contiguousSize=33554432
U-Boot > saveenv
 

After the Android logo on the display ends, it auto reboots as soon as a lock screen displays!

here is debug log

\0\0\0

U-Boot 2017.03 (Jan 20 2018 - 10:42:40 +0800)

CPU: Freescale i.MX6Q rev1.2 996 MHz (running at 792 MHz)
CPU: Automotive temperature grade (-40C to 125C) at 37C
Reset cause: POR
Model: Freescale i.MX6 Quad SABRE Smart Device Board
Board: MX6-SabreSD
DRAM: 1 GiB
PMIC: PFUZE100! DEV_ID=0x10 REV_ID=0x21
MMC: FSL_SDHC: 0, FSL_SDHC: 1, FSL_SDHC: 2
No panel detected: default to Hannstar-XGA
Display: Hannstar-XGA (1024x768)
In: serial
Out: serial
Err: serial
flash target is MMC:1
Net: eth0: ethernet@02188000 [PRIME]
Fastboot: Normal
Hit any key to stop autoboot: 3  2  1  0 
boota mmc1 
kernel @ 14008000 (9966584)
ramdisk @ 15000000 (2038058)
fdt @ 14f00000 (50925)
## Booting Android Image at 0x12000000 ...
Kernel load addr 0x14008000 size 9733 KiB
Kernel command line: console=ttymxc0,115200 androidboot.console=ttymxc0 consoleblank=0 vmalloc=128M init=/init video=mxcfb0:dev=hdmi,1920x1080M@60,bpp=32 video=mxcfb1:off video=mxcfb2:off video=mxcfb3:off androidboot.hardware=freescale cma=448M galcore.contiguousSize=33554432 androidboot.serialno=061279d4e6b34649 androidboot.soc_type=imx6q androidboot.storage_type=sd gpt
## Flattened Device Tree blob at 14f00000
Booting using the fdt blob at 0x14f00000
Loading Kernel Image ... OK
Using Device Tree in place at 14f00000, end 14f0f6ec
switch to ldo_bypass mode!

Starting kernel ...

Booting Linux on physical CPU 0x0
Linux version 4.9.17-00009-ga88711e (bamboo@shlinux23) (gcc version 4.9.x 20150123 (prerelease) (GCC) ) #1 SMP PREEMPT Sat Jan 20 10:45:22 CST 2018
CPU: ARMv7 Processor [412fc09a] revision 10 (ARMv7), cr=10c53c7d
CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache
OF: fdt:Machine model: Freescale i.MX6 Quad SABRE Smart Device Board
cma: Reserved 448 MiB at 0x2a000000
Memory policy: Data cache writealloc
percpu: Embedded 15 pages/cpu @f6eb6000 s31040 r8192 d22208 u61440
Built 1 zonelists in Zone order, mobility grouping on. Total pages: 260368
Kernel command line: console=ttymxc0,115200 androidboot.console=ttymxc0 consoleblank=0 vmalloc=128M init=/init video=mxcfb0:dev=hdmi,1920x1080M@60,bpp=32 video=mxcfb1:off video=mxcfb2:off video=mxcfb3:off androidboot.hardware=freescale cma=448M galcore.contiguousSize=33554432 androidboot.serialno=061279d4e6b34649 androidboot.soc_type=imx6q androidboot.storage_type=sd gpt
PID hash table entries: 4096 (order: 2, 16384 bytes)
Dentry cache hash table entries: 131072 (order: 7, 524288 bytes)
Inode-cache hash table entries: 65536 (order: 6, 262144 bytes)
Memory: 556280K/1048576K available (13312K kernel code, 1121K rwdata, 4296K rodata, 1024K init, 612K bss, 33544K reserved, 458752K cma-reserved, 139264K highmem)
Virtual kernel memory layout:
vector : 0xffff0000 - 0xffff1000 ( 4 kB)
fixmap : 0xffc00000 - 0xfff00000 (3072 kB)
vmalloc : 0xf8000000 - 0xff800000 ( 120 MB)
lowmem : 0xc0000000 - 0xf7800000 ( 888 MB)
pkmap : 0xbfe00000 - 0xc0000000 ( 2 MB)
modules : 0xbf000000 - 0xbfe00000 ( 14 MB)
.text : 0xc0008000 - 0xc0e00000 (14304 kB)
.init : 0xc1300000 - 0xc1400000 (1024 kB)
.data : 0xc1400000 - 0xc1518718 (1122 kB)
.bss : 0xc1518718 - 0xc15b18a0 ( 613 kB)
SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=4, Nodes=1
Preemptible hierarchical RCU implementation.
Build-time adjustment of leaf fanout to 32.
NR_IRQS:16 nr_irqs:16 16
L2C-310 errata 752271 769419 enabled
L2C-310 enabling early BRESP for Cortex-A9
L2C-310 full line of zeros enabled for Cortex-A9
L2C-310 ID prefetch enabled, offset 16 lines
L2C-310 dynamic clock gating enabled, standby mode enabled
L2C-310 cache controller enabled, 16 ways, 1024 kB
L2C-310: CACHE_ID 0x410000c7, AUX_CTRL 0x76470001
Switching to timer-based delay loop, resolution 333ns
sched_clock: 32 bits at 3000kHz, resolution 333ns, wraps every 715827882841ns
clocksource: mxc_timer1: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 637086815595 ns
Console: colour dummy device 80x30
Calibrating delay loop (skipped), value calculated using timer frequency.. 6.00 BogoMIPS (lpj=30000)
pid_max: default: 32768 minimum: 301
Security Framework initialized
SELinux: Initializing.
Mount-cache hash table entries: 2048 (order: 1, 8192 bytes)
Mountpoint-cache hash table entries: 2048 (order: 1, 8192 bytes)
CPU: Testing write buffer coherency: ok
CPU0: update cpu_capacity 1024
CPU0: thread -1, cpu 0, socket 0, mpidr 80000000
Setting up static identity map for 0x10100000 - 0x10100058
CPU1: update cpu_capacity 1024
CPU1: thread -1, cpu 1, socket 0, mpidr 80000001
CPU2: update cpu_capacity 1024
CPU2: thread -1, cpu 2, socket 0, mpidr 80000002
CPU3: update cpu_capacity 1024
CPU3: thread -1, cpu 3, socket 0, mpidr 80000003
Brought up 4 CPUs
SMP: Total of 4 processors activated (24.00 BogoMIPS).
CPU: All CPU(s) started in SVC mode.
CPU3: update max cpu_capacity 1024
devtmpfs: initialized
CPU2: update max cpu_capacity 1024
VFP support v0.3: implementor 41 architecture 3 part 30 variant 9 rev 4
clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 19112604462750000 ns
futex hash table entries: 1024 (order: 4, 65536 bytes)
pinctrl core: initialized pinctrl subsystem
NET: Registered protocol family 16
DMA: preallocated 256 KiB pool for atomic coherent allocations
cpuidle: using governor menu
CPU identified as i.MX6Q, silicon rev 1.2
vddarm: bypassed regulator has no supply!
vddarm: failed to get the current voltage(-517)
vddsoc: bypassed regulator has no supply!
vddsoc: failed to get the current voltage(-517)
hw-breakpoint: found 5 (+1 reserved) breakpoint and 1 watchpoint registers.
hw-breakpoint: maximum watchpoint size is 4 bytes.
imx6q-pinctrl 20e0000.iomuxc: initialized IMX pinctrl driver
imx-gpc 20dc000.gpc: pu regulator not ready, retry
mxs-dma 110000.dma-apbh: initialized
SCSI subsystem initialized
usbcore: registered new interface driver usbfs
usbcore: registered new interface driver hub
usbcore: registered new device driver usb
2000000.aips-bus:usbphy_nop1 supply vcc not found, using dummy regulator
2000000.aips-bus:usbphy_nop2 supply vcc not found, using dummy regulator
i2c i2c-0: IMX I2C adapter registered
i2c i2c-0: can't use DMA, using PIO instead.
i2c i2c-1: IMX I2C adapter registered
i2c i2c-1: can't use DMA, using PIO instead.
i2c i2c-2: IMX I2C adapter registered
i2c i2c-2: can't use DMA, using PIO instead.
Linux video capture interface: v2.00
pps_core: LinuxPPS API ver. 1 registered
pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it>
PTP clock support registered
imx-ipuv3 2400000.ipu: IPU DMFC NORMAL mode: 1(0~1), 5B(4,5), 5F(6,7)
imx-ipuv3 2800000.ipu: IPU DMFC NORMAL mode: 1(0~1), 5B(4,5), 5F(6,7)
mxc_mipi_csi2 21dc000.mipi_csi: i.MX MIPI CSI2 driver probed
mxc_mipi_csi2 21dc000.mipi_csi: i.MX MIPI CSI2 dphy version is 0x3130302a
MIPI CSI2 driver module loaded
imx rpmsg driver is registered.
Advanced Linux Sound Architecture Driver Initialized.
Bluetooth: Core ver 2.22
NET: Registered protocol family 31
Bluetooth: HCI device and connection manager initialized
Bluetooth: HCI socket layer initialized
Bluetooth: L2CAP socket layer initialized
Bluetooth: SCO socket layer initialized
clocksource: Switched to clocksource mxc_timer1
VFS: Disk quotas dquot_6.6.0
VFS: Dquot-cache hash table entries: 1024 (order 0, 4096 bytes)
NET: Registered protocol family 2
TCP established hash table entries: 8192 (order: 3, 32768 bytes)
TCP bind hash table entries: 8192 (order: 4, 65536 bytes)
TCP: Hash tables configured (established 8192 bind 8192)
UDP hash table entries: 512 (order: 2, 16384 bytes)
UDP-Lite hash table entries: 512 (order: 2, 16384 bytes)
NET: Registered protocol family 1
RPC: Registered named UNIX socket transport module.
RPC: Registered udp transport module.
RPC: Registered tcp transport module.
RPC: Registered tcp NFSv4.1 backchannel transport module.
Trying to unpack rootfs image as initramfs...
Freeing initrd memory: 1992K (c5000000 - c51f2000)
hw perfevents: enabled with armv7_cortex_a9 PMU driver, 7 counters available
Bus freq driver module loaded
bt power gpio is:2
rfkill: BT RF going to : on
mxc_bt_rfkill_reset
mxc_bt_rfkill driver success loaded
audit: initializing netlink subsys (disabled)
audit: type=2000 audit(0.780:1): initialized
workingset: timestamp_bits=30 max_order=18 bucket_order=0
Registering sdcardfs 0.1
NFS: Registering the id_resolver key type
Key type id_resolver registered
Key type id_legacy registered
ntfs: driver 2.1.32 [Flags: R/W DEBUG].
jffs2: version 2.2. (NAND) © 2001-2006 Red Hat, Inc.
fuse init (API version 7.26)
bounce: pool size: 64 pages
io scheduler noop registered
io scheduler deadline registered
io scheduler cfq registered (default)
imx-weim 21b8000.weim: Driver registered.
backlight supply power not found, using dummy regulator
mxc_mipi_dsi 21e0000.mipi: i.MX MIPI DSI driver probed
mxc_hdmi 20e0000.hdmi_video: Detected HDMI controller 0x13:0xa:0xa0:0xc1
fbcvt: 1920x1080@60: CVT Name - 2.073M9
mxc_sdc_fb fb@0: registered mxc display driver hdmi
imx-ipuv3 2400000.ipu: IPU DMFC DP HIGH RESOLUTION: 1(0,1), 5B(2~5), 5F(6,7)
Console: switching to colour frame buffer device 240x67
mxc_sdc_fb fb@1: Can't get fb option for mxcfb1!
mxc_sdc_fb fb@2: Can't get fb option for mxcfb2!
mxc_sdc_fb fb@3: Can't get fb option for mxcfb3!
imx-sdma 20ec000.sdma: no iram assigned, using external mem
imx-sdma 20ec000.sdma: loaded firmware 3.3
pfuze100-regulator 1-0008: Full layer: 2, Metal layer: 1
pfuze100-regulator 1-0008: FAB: 0, FIN: 0
pfuze100-regulator 1-0008: pfuze100 found.
vddpu: supplied by SW1C
usb_otg_vbus: supplied by SWBST
usb_h1_vbus: supplied by SWBST
2020000.serial: ttymxc0 at MMIO 0x2020000 (irq = 27, base_baud = 5000000) is a IMX
console [ttymxc0] enabled
21f4000.serial: ttymxc4 at MMIO 0x21f4000 (irq = 76, base_baud = 5000000) is a IMX
imx sema4 driver is registered.
[drm] Initialized
[drm] Initialized vivante 1.0.0 20120216 on minor 0
brd: module loaded
loop: module loaded
zram: Added device: zram0
libphy: Fixed MDIO Bus: probed
tun: Universal TUN/TAP device driver, 1.6
tun: (C) 1999-2004 Max Krasnyansky <maxk@qualcomm.com>
CAN device driver interface
2188000.ethernet supply phy not found, using dummy regulator
pps pps0: new PPS source ptp0
libphy: fec_enet_mii_bus: probed
fec 2188000.ethernet eth0: registered PHC device 0
PPP generic driver version 2.4.2
PPP BSD Compression module registered
PPP Deflate Compression module registered
PPP MPPE Compression module registered
NET: Registered protocol family 24
usbcore: registered new interface driver kaweth
pegasus: v0.9.3 (2013/04/25), Pegasus/Pegasus II USB Ethernet driver
usbcore: registered new interface driver pegasus
usbcore: registered new interface driver rtl8150
usbcore: registered new interface driver r8152
usbcore: registered new interface driver asix
usbcore: registered new interface driver ax88179_178a
usbcore: registered new interface driver cdc_ether
usbcore: registered new interface driver cdc_eem
usbcore: registered new interface driver net1080
usbcore: registered new interface driver cdc_subset
usbcore: registered new interface driver zaurus
usbcore: registered new interface driver cdc_ncm
ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver
ehci-mxc: Freescale On-Chip EHCI Host driver
usbcore: registered new interface driver cdc_acm
cdc_acm: USB Abstract Control Model driver for USB modems and ISDN adapters
usbcore: registered new interface driver usb-storage
usbcore: registered new interface driver usbserial
usbcore: registered new interface driver usbserial_generic
usbserial: USB Serial support registered for generic
usbcore: registered new interface driver ftdi_sio
usbserial: USB Serial support registered for FTDI USB Serial Device
usbcore: registered new interface driver option
usbserial: USB Serial support registered for GSM modem (1-port)
usbcore: registered new interface driver usbtest
usbcore: registered new interface driver usb_ehset_test
2184800.usbmisc supply vbus-wakeup not found, using dummy regulator
ci_hdrc ci_hdrc.1: EHCI Host Controller
ci_hdrc ci_hdrc.1: new USB bus registered, assigned bus number 1
ci_hdrc ci_hdrc.1: USB 2.0 started, EHCI 1.00
usb usb1: New USB device found, idVendor=1d6b, idProduct=0002
usb usb1: New USB device strings: Mfr=3, Product=2, SerialNumber=1
usb usb1: Product: EHCI Host Controller
usb usb1: Manufacturer: Linux 4.9.17-00009-ga88711e ehci_hcd
usb usb1: SerialNumber: ci_hdrc.1
hub 1-0:1.0: USB hub found
hub 1-0:1.0: 1 port detected
mousedev: PS/2 mouse device common for all mice
usbcore: registered new interface driver xpad
usbcore: registered new interface driver usb_acecad
usbcore: registered new interface driver aiptek
usbcore: registered new interface driver gtco
usbcore: registered new interface driver hanwang
usbcore: registered new interface driver kbtab
egalax_ts 1-0004: Failed to switch to I2C interface
egalax_ts 2-0004: Failed to switch to I2C interface
egalax_ts: probe of 2-0004 failed with error -110
input: max11801_ts as /devices/soc0/soc/2100000.aips-bus/21a4000.i2c/i2c-1/1-0048/input/input2
snvs_rtc 20cc000.snvs:snvs-rtc-lp: rtc core: registered 20cc000.snvs:snvs-r as rtc0
i2c /dev entries driver
IR NEC protocol handler initialized
IR RC5(x/sz) protocol handler initialized
IR RC6 protocol handler initialized
IR JVC protocol handler initialized
IR Sony protocol handler initialized
IR SANYO protocol handler initialized
IR Sharp protocol handler initialized
IR MCE Keyboard/mouse protocol handler initialized
IR XMP protocol handler initialized
mxc_v4l2_output v4l2_out: V4L2 device registered as video16
mxc_v4l2_output v4l2_out: V4L2 device registered as video17
ov5640_read_reg:write reg error:reg=300a
camera ov5640 is not found
ov5642_read_reg:write reg error:reg=300a
camera ov5642 is not found
ov5640_read_reg:write reg error:reg=300a
camera ov5640_mipi is not found
usbcore: registered new interface driver uvcvideo
USB Video Class driver (1.1.1)
mag3110 2-000e: check mag3110 chip ID
input: FreescaleMagnetometer as /devices/virtual/input/input3
input: eCompass as /devices/virtual/input/input4
mag3110 2-000e: mag3110 is probed
input: FreescaleAccelerometer as /devices/virtual/input/input5
mma8x5x device driver probe successfully
imx2-wdt 20c0000.wdog: timeout 60 sec (nowayout=0)
device-mapper: uevent: version 1.0.3
device-mapper: ioctl: 4.35.0-ioctl (2016-06-23) initialised: dm-devel@redhat.com
Bluetooth: HCI UART driver ver 2.3
Bluetooth: HCI UART protocol H4 registered
Bluetooth: HCI UART protocol BCSP registered
Bluetooth: HCI UART protocol ATH3K registered
usbcore: registered new interface driver btusb
sdhci: Secure Digital Host Controller Interface driver
sdhci: Copyright(c) Pierre Ossman
sdhci-pltfm: SDHCI platform and OF driver helper
sdhci-esdhc-imx 2194000.usdhc: Got WP GPIO
sdhci-esdhc-imx 2194000.usdhc: assigned as wifi host
mmc1: SDHCI controller on 2194000.usdhc [2194000.usdhc] using ADMA
sdhci-esdhc-imx 2198000.usdhc: Got CD GPIO
sdhci-esdhc-imx 2198000.usdhc: Got WP GPIO
mmc2: SDHCI controller on 2198000.usdhc [2198000.usdhc] using ADMA
random: fast init done
mmc2: new high speed SDHC card at address aaaa
mmcblk2: mmc2:aaaa SS08G 7.40 GiB 
mmc3: SDHCI controller on 219c000.usdhc [219c000.usdhc] using ADMA
mxc_vdoa 21e4000.vdoa: i.MX Video Data Order Adapter(VDOA) driver probed
mxc_hdmi_cec soc:hdmi_cec@00120000: HDMI CEC initialized
leds-gpio: probe of leds failed with error -16
caam 2100000.caam: ERA source: CAAMVID.
caam 2100000.caam: AXI pipeline throttling enabled.
caam 2100000.caam: Instantiated RNG4 SH1
caam 2100000.caam: device ID = 0x0a16010000000000 (Era 4)
caam 2100000.caam: job rings = 2, qi = 0
Primary GPT is invalid, using alternate GPT.
mmcblk2: p1 p2 p3 p4 p5 p6 p7 p8 p9 p10 p11
caam algorithms registered in /proc/crypto
caam_jr 2101000.jr0: registering rng-caam
platform caam_sm: blkkey_ex: 4 keystore units available
platform caam_sm: 64-bit clear key:
platform caam_sm: [0000] 00 01 02 03 04 0f 06 07
platform caam_sm: 64-bit black key:
platform caam_sm: [0000] 6d 01 50 e7 be 5b e6 d9
platform caam_sm: [0008] 30 99 9d 3b 9d 39 af 57
platform caam_sm: 128-bit clear key:
platform caam_sm: [0000] 00 01 02 03 04 0f 06 07
platform caam_sm: [0008] 08 09 0a 0b 0c 0d 0e 0f
platform caam_sm: 128-bit black key:
platform caam_sm: [0000] 68 3d 76 50 05 d7 b0 f1
platform caam_sm: [0008] 38 a2 44 6b 78 4c bd b1
platform caam_sm: 192-bit clear key:
platform caam_sm: [0000] 00 01 02 03 04 0f 06 07
platform caam_sm: [0008] 08 09 0a 0b 0c 0d 0e 0f
platform caam_sm: [0016] 10 11 12 13 14 15 16 17
platform caam_sm: 192-bit black key:
platform caam_sm: [0000] f7 8f 0a a3 ca d3 84 96
platform caam_sm: [0008] bf 16 95 89 64 8e 3a 68
platform caam_sm: [0016] 1a 34 90 c7 a3 b3 c1 5b
platform caam_sm: [0024] 6e f0 65 5c ec 8a 51 99
platform caam_sm: 256-bit clear key:
platform caam_sm: [0000] 00 01 02 03 04 0f 06 07
platform caam_sm: [0008] 08 09 0a 0b 0c 0d 0e 0f
platform caam_sm: [0016] 10 11 12 13 14 15 16 17
platform caam_sm: [0024] 18 19 1a 1b 1c 1d 1e 1f
platform caam_sm: 256-bit black key:
platform caam_sm: [0000] 5b 5b 00 84 01 90 48 ac
platform caam_sm: [0008] 63 bf d4 13 71 89 25 fe
platform caam_sm: [0016] f6 ec 25 dc 40 1a 3f 1c
platform caam_sm: [0024] 92 8e 6f 5d 22 e0 8c d2
platform caam_sm: 64-bit unwritten blob:
platform caam_sm: [0000] 00 00 00 00 00 00 00 00
platform caam_sm: [0008] 00 00 00 00 00 00 00 00
platform caam_sm: [0016] 00 00 00 00 00 00 00 00
platform caam_sm: [0024] 00 00 00 00 00 00 00 00
platform caam_sm: [0032] 00 00 00 00 00 00 00 00
platform caam_sm: [0040] 00 00 00 00 00 00 00 00
platform caam_sm: [0048] 00 00 00 00 00 00 00 00
mmc3: new DDR MMC card at address 0001
mmcblk3: mmc3:0001 SEM08G 7.40 GiB 
platform caam_sm: [0056] 00 00 00 00 00 00 00 00
platform caam_sm: [0064] 00 00 00 00 00 00 00 00
platform caam_sm: [0072] 00 00 00 00 00 00 00 00
mmcblk3boot0: mmc3:0001 SEM08G partition 1 2.00 MiB
mmcblk3boot1: mmc3:0001 SEM08G partition 2 2.00 MiB
mmcblk3rpmb: mmc3:0001 SEM08G partition 3 128 KiB
Alternate GPT is invalid, using primary GPT.
mmcblk3: p1 p2 p3 p4 p5 p6 p7 p8 p9 p10 p11
platform caam_sm: [0080] 00 00 00 00 00 00 00 00
platform caam_sm: [0088] 00 00 00 00 00 00 00 00
platform caam_sm: 128-bit unwritten blob:
platform caam_sm: [0000] 00 00 00 00 00 00 00 00
platform caam_sm: [0008] 00 00 00 00 00 00 00 00
platform caam_sm: [0016] 00 00 00 00 00 00 00 00
platform caam_sm: [0024] 00 00 00 00 00 00 00 00
platform caam_sm: [0032] 00 00 00 00 00 00 00 00
platform caam_sm: [0040] 00 00 00 00 00 00 00 00
platform caam_sm: [0048] 00 00 00 00 00 00 00 00
platform caam_sm: [0056] 00 00 00 00 00 00 00 00
platform caam_sm: [0064] 00 00 00 00 00 00 00 00
platform caam_sm: [0072] 00 00 00 00 00 00 00 00
platform caam_sm: [0080] 00 00 00 00 00 00 00 00
platform caam_sm: [0088] 00 00 00 00 00 00 00 00
platform caam_sm: 196-bit unwritten blob:
platform caam_sm: [0000] 00 00 00 00 00 00 00 00
platform caam_sm: [0008] 00 00 00 00 00 00 00 00
platform caam_sm: [0016] 00 00 00 00 00 00 00 00
platform caam_sm: [0024] 00 00 00 00 00 00 00 00
platform caam_sm: [0032] 00 00 00 00 00 00 00 00
platform caam_sm: [0040] 00 00 00 00 00 00 00 00
platform caam_sm: [0048] 00 00 00 00 00 00 00 00
platform caam_sm: [0056] 00 00 00 00 00 00 00 00
platform caam_sm: [0064] 00 00 00 00 00 00 00 00
platform caam_sm: [0072] 00 00 00 00 00 00 00 00
platform caam_sm: [0080] 00 00 00 00 00 00 00 00
platform caam_sm: [0088] 00 00 00 00 00 00 00 00
platform caam_sm: 256-bit unwritten blob:
platform caam_sm: [0000] 00 00 00 00 00 00 00 00
platform caam_sm: [0008] 00 00 00 00 00 00 00 00
platform caam_sm: [0016] 00 00 00 00 00 00 00 00
platform caam_sm: [0024] 00 00 00 00 00 00 00 00
platform caam_sm: [0032] 00 00 00 00 00 00 00 00
platform caam_sm: [0040] 00 00 00 00 00 00 00 00
platform caam_sm: [0048] 00 00 00 00 00 00 00 00
platform caam_sm: [0056] 00 00 00 00 00 00 00 00
platform caam_sm: [0064] 00 00 00 00 00 00 00 00
platform caam_sm: [0072] 00 00 00 00 00 00 00 00
platform caam_sm: [0080] 00 00 00 00 00 00 00 00
platform caam_sm: [0088] 00 00 00 00 00 00 00 00
platform caam_sm: 64-bit black key in blob:
platform caam_sm: [0000] d2 cf 33 1c 35 74 66 50
platform caam_sm: [0008] 9c 2c 5e f1 2d 93 1c fc
platform caam_sm: [0016] 79 fc e7 e9 62 ce ea 40
platform caam_sm: [0024] ee e6 a4 06 cd 50 e8 c7
platform caam_sm: [0032] 07 b4 2c 9a 3d 8c f3 e0
platform caam_sm: [0040] 15 e7 cd f8 e4 24 4c cf
platform caam_sm: [0048] 78 3d 43 98 6d a2 32 1b
platform caam_sm: [0056] 00 00 00 00 00 00 00 00
platform caam_sm: [0064] 00 00 00 00 00 00 00 00
platform caam_sm: [0072] 00 00 00 00 00 00 00 00
platform caam_sm: [0080] 00 00 00 00 00 00 00 00
platform caam_sm: [0088] 00 00 00 00 00 00 00 00
platform caam_sm: 128-bit black key in blob:
platform caam_sm: [0000] 88 16 ae a4 55 25 b9 be
platform caam_sm: [0008] b7 37 4d ac 76 1f d7 73
platform caam_sm: [0016] 97 a4 dc a3 09 c6 67 29
platform caam_sm: [0024] 95 e6 be a1 95 59 a4 c1
platform caam_sm: [0032] 3c 14 38 75 14 59 10 93
platform caam_sm: [0040] 01 c4 9d 13 24 19 1b 00
platform caam_sm: [0048] 94 f4 47 b5 90 fb 77 78
platform caam_sm: [0056] 3f 00 90 48 2d 6f 23 04
platform caam_sm: [0064] 00 00 00 00 00 00 00 00
platform caam_sm: [0072] 00 00 00 00 00 00 00 00
platform caam_sm: [0080] 00 00 00 00 00 00 00 00
platform caam_sm: [0088] 00 00 00 00 00 00 00 00
platform caam_sm: 192-bit black key in blob:
platform caam_sm: [0000] 79 91 f4 a4 84 9a 7f 19
platform caam_sm: [0008] d3 7d 95 c8 72 c4 42 0c
platform caam_sm: [0016] 05 5f 47 f1 3d 29 e2 41
platform caam_sm: [0024] 9d 94 ba a8 31 68 b4 72
platform caam_sm: [0032] 7b a2 4e 27 4b 78 ef db
platform caam_sm: [0040] 7d 48 3e b2 c0 6b 1c 2d
platform caam_sm: [0048] d8 3f 4f 50 ef ad ad 5d
platform caam_sm: [0056] f2 2a ce 94 b5 d2 8f 95
platform caam_sm: [0064] 7a b7 44 e1 1d 55 33 3d
platform caam_sm: [0072] 00 00 00 00 00 00 00 00
platform caam_sm: [0080] 00 00 00 00 00 00 00 00
platform caam_sm: [0088] 00 00 00 00 00 00 00 00
platform caam_sm: 256-bit black key in blob:
platform caam_sm: [0000] 63 f1 8f 38 a6 ac 0e 08
platform caam_sm: [0008] 4b 7c 5b a0 02 5f ce 4f
platform caam_sm: [0016] 4c 4b b6 94 1c b5 87 aa
platform caam_sm: [0024] d6 92 ec 0b ae bf 15 79
platform caam_sm: [0032] 62 9c 0f df ad 59 24 91
platform caam_sm: [0040] 09 a0 e8 29 e1 72 aa 5e
platform caam_sm: [0048] b8 18 4f 7f 38 37 5b 6a
platform caam_sm: [0056] ab 49 d8 d7 ab 86 89 32
platform caam_sm: [0064] 7b 4b 16 ed d9 8b fb d2
platform caam_sm: [0072] b2 5a 85 3d 01 18 d3 15
platform caam_sm: [0080] 00 00 00 00 00 00 00 00
platform caam_sm: [0088] 00 00 00 00 00 00 00 00
platform caam_sm: restored 64-bit black key:
platform caam_sm: [0000] 63 e6 89 bf dc c1 bb c3
platform caam_sm: [0008] 47 c1 ca 67 75 e6 9a dd
platform caam_sm: restored 128-bit black key:
platform caam_sm: [0000] 68 3d 76 50 05 d7 b0 f1
platform caam_sm: [0008] 38 a2 44 6b 78 4c bd b1
platform caam_sm: restored 192-bit black key:
platform caam_sm: [0000] f7 8f 0a a3 ca d3 84 96
platform caam_sm: [0008] bf 16 95 89 64 8e 3a 68
platform caam_sm: [0016] 6f 2e 04 2e 0f ce 69 04
platform caam_sm: [0024] bf 46 5e 19 da a7 1d 11
platform caam_sm: restored 256-bit black key:
platform caam_sm: [0000] 5b 5b 00 84 01 90 48 ac
platform caam_sm: [0008] 63 bf d4 13 71 89 25 fe
platform caam_sm: [0016] f6 ec 25 dc 40 1a 3f 1c
platform caam_sm: [0024] 92 8e 6f 5d 22 e0 8c d2
snvs-secvio 20cc000.caam-snvs: can't get snvs clock
snvs-secvio 20cc000.caam-snvs: violation handlers armed - non-secure state
caam_keyblob caam_keyblob: caam keyblob initialized
hidraw: raw HID events driver (C) Jiri Kosina
usbcore: registered new interface driver usbhid
usbhid: USB HID core driver
ion_parse_dt_heap_common: id 0 type 4 name cma align 1000
ion_parse_dt_heap_common: id 1 type 1 name sys-contig align 1000
ion_parse_dt_heap_common: id 2 type 0 name system align 1000
ashmem: initialized
usbcore: registered new interface driver snd-usb-audio
wm8962 0-001a: customer id 0 revision D
fsl-ssi-dai 202c000.ssi: No cache defaults, reading back from HW
input: WM8962 Beep Generator as /devices/soc0/soc/2100000.aips-bus/21a0000.i2c/i2c-0/0-001a/input/input6
imx-wm8962 sound: wm8962 <-> 202c000.ssi mapping ok
imx-wm8962 sound: snd-soc-dummy-dai <-> 2034000.asrc mapping ok
imx-wm8962 sound: wm8962 <-> 202c000.ssi mapping ok
imx-audio-hdmi sound-hdmi: hdmi-hifi.0 <-> soc:hdmi_audio@00120000 mapping ok
NET: Registered protocol family 26
u32 classifier
Actions configured
Netfilter messages via NETLINK v0.30.
nf_conntrack version 0.5.0 (16384 buckets, 65536 max)
ctnetlink v0.93: registering with nfnetlink.
xt_time: kernel timezone is -0000
ip_tables: (C) 2000-2006 Netfilter Core Team
arp_tables: arp_tables: (C) 2002 David S. Miller
Initializing XFRM netlink socket
NET: Registered protocol family 10
mip6: Mobile IPv6
ip6_tables: (C) 2000-2006 Netfilter Core Team
sit: IPv6, IPv4 and MPLS over IPv4 tunneling driver
NET: Registered protocol family 17
NET: Registered protocol family 15
can: controller area network core (rev 20120528 abi 9)
NET: Registered protocol family 29
can: raw protocol (rev 20120528)
can: broadcast manager protocol (rev 20161123 t)
can: netlink gateway (rev 20130117) max_hops=1
Bluetooth: RFCOMM TTY layer initialized
Bluetooth: RFCOMM socket layer initialized
Bluetooth: RFCOMM ver 1.11
Bluetooth: BNEP (Ethernet Emulation) ver 1.3
Bluetooth: BNEP filters: protocol multicast
Bluetooth: BNEP socket layer initialized
Bluetooth: HIDP (Human Interface Emulation) ver 1.2
Bluetooth: HIDP socket layer initialized
8021q: 802.1Q VLAN Support v1.8
Key type dns_resolver registered
cpu cpu0: regulators not ready, retry
registered taskstats version 1
vddarm: supplied by SW1AB
vddsoc: supplied by SW1C
imx-gpc 20dc000.gpc: Registered imx-gpc
mxc_vpu 2040000.vpu_fsl: VPU initialized
Galcore version 6.2.2.96445
cpu cpu0: Registered imx6q-cpufreq
imx_thermal 2000000.aips-bus:tempmon: Automotive CPU temperature grade - max:125C critical:120C passive:115C
dhd_module_init in
wifi_plat_dev_drv_probe no GPIO for OOB in device tree.
wifi_plat_dev_drv_probe continue with non-OOB mode.
Power-up adapter 'DHD generic adapter'
wifi_platform_bus_enumerate device present 1
failed to power up DHD generic adapter, 3 retry left
wifi_platform_bus_enumerate device present 0
wifi_platform_bus_enumerate device present 1
failed to power up DHD generic adapter, 2 retry left
wifi_platform_bus_enumerate device present 0
wifi_platform_bus_enumerate device present 1
failed to power up DHD generic adapter, 1 retry left
wifi_platform_bus_enumerate device present 0
wifi_platform_bus_enumerate device present 1
failed to power up DHD generic adapter, 0 retry left
wifi_platform_bus_enumerate device present 0
failed to power up DHD generic adapter, max retry reached**
input: gpio-keys as /devices/soc0/gpio-keys/input/input9
snvs_rtc 20cc000.snvs:snvs-rtc-lp: setting system clock to 1970-01-01 00:18:28 UTC (1108)
usb_otg_vbus: disabling
wm8962-supply: disabling
wlreg_on: disabling
SW4: disabling
VGEN1: disabling
ALSA device list:
#0: wm8962-audio
#1: imx-hdmi-soc
Freeing unused kernel memory: 1024K (c1300000 - c1400000)
init: init first stage started!
init: First stage mount skipped (missing/incompatible fstab in device tree)
init: Skipped setting INIT_AVB_VERSION (not in recovery mode)
init: Loading SELinux policy
SELinux: Permission validate_trans in class security not defined in policy.
SELinux: the above unknown classes and permissions will be denied
audit: type=1403 audit(1108.650:2): policy loaded auid=4294967295 ses=4294967295
selinux: SELinux: Loaded policy from /sepolicy

audit: type=1404 audit(1108.670:3): enforcing=1 old_enforcing=0 auid=4294967295 ses=4294967295
selinux: SELinux: Loaded file_contexts

init: init second stage started!
selinux: SELinux: Loaded file_contexts

selinux: SELinux: Loaded property_contexts from /plat_property_contexts & /nonplat_property_contexts.

init: Running restorecon...
selinux: SELinux: Could not stat /dev/block: No such file or directory.

init: waitpid failed: No child processes
init: Couldn't load property file: Unable to open '/system/etc/prop.default': No such file or directory: No such file or directory
init: Couldn't load property file: Unable to open '/prop.default': No such file or directory: No such file or directory
init: Couldn't load property file: Unable to open '/odm/default.prop': No such file or directory: No such file or directory
init: Couldn't load property file: Unable to open '/vendor/default.prop': No such file or directory: No such file or directory
ueventd: ueventd started!
ueventd: Parsing file /ueventd.rc...
ueventd: Parsing file /vendor/ueventd.rc...
ueventd: Unable to open '/vendor/ueventd.rc': No such file or directory
ueventd: Parsing file /odm/ueventd.rc...
ueventd: Unable to open '/odm/ueventd.rc': No such file or directory
ueventd: Parsing file /ueventd.freescale.rc...
selinux: SELinux: Loaded file_contexts

selinux: SELinux: Loaded file_contexts

ueventd: Coldboot took 0.263877 seconds
keychord: using input dev gpio-keys for fevent
Console: switching to colour dummy device 80x30
watchdogd: watchdogd started (interval 10, margin 20)!
fec: <231> warning: __ecc_read: RS block 5263360: decoding failed
fec: <233> warning: __ecc_read: RS block 5263360: decoding failed
fec: <236> warning: __ecc_read: RS block 5263360: decoding failed
EXT4-fs (dm-0): mounted filesystem with ordered data mode. Opts: barrier=1
EXT4-fs (mmcblk2p10): Ignoring removed nomblk_io_submit option
EXT4-fs (mmcblk2p10): recovery complete
EXT4-fs (mmcblk2p10): mounted filesystem with ordered data mode. Opts: errors=remount-ro,nomblk_io_submit
init: [libfs_mgr]check_fs(): mount(/dev/block/by-name/userdata,/data,ext4)=0: Success
init: [libfs_mgr]check_fs(): unmount(/data) succeeded
init: [libfs_mgr]Running /system/bin/e2fsck on /dev/block/by-name/userdata
e2fsck: e2fsck 1.43.3 (04-Sep-2016)

e2fsck: Pass 1: Checking inodes, blocks, and sizes

e2fsck: Pass 2: Checking directory structure

e2fsck: Pass 3: Checking directory connectivity

e2fsck: Pass 4: Checking reference counts

e2fsck: Pass 5: Checking group summary information

e2fsck:

e2fsck: /dev/block/by-name/userdata: ***** FILE SYSTEM WAS MODIFIED *****

e2fsck: /dev/block/by-name/userdata: 1217/315120 files (2.6% non-contiguous), 60336/1260032 blocks

EXT4-fs (mmcblk2p10): Ignoring removed nomblk_io_submit option
EXT4-fs (mmcblk2p10): mounted filesystem with ordered data mode. Opts: nomblk_io_submit,noauto_da_alloc,errors=panic
init: [libfs_mgr]__mount(source=/dev/block/by-name/userdata,target=/data,type=ext4)=0
init: [libfs_mgr]superblock s_max_mnt_count:65535,/dev/block/by-name/cache
init: [libfs_mgr]do_quota_with_shutdown_check(): was not clealy shutdown, state flag:1incompat flag:246
init: [libfs_mgr]Requested quota status is match on /dev/block/by-name/cache
EXT4-fs (mmcblk2p4): Ignoring removed nomblk_io_submit option
EXT4-fs (mmcblk2p4): recovery complete
EXT4-fs (mmcblk2p4): mounted filesystem with ordered data mode. Opts: errors=remount-ro,nomblk_io_submit
init: [libfs_mgr]check_fs(): mount(/dev/block/by-name/cache,/cache,ext4)=0: Success
init: [libfs_mgr]check_fs(): unmount(/cache) succeeded
init: [libfs_mgr]Running /system/bin/e2fsck on /dev/block/by-name/cache
e2fsck: e2fsck 1.43.3 (04-Sep-2016)

EXT4-fs (mmcblk2p4): Ignoring removed nomblk_io_submit option
EXT4-fs (mmcblk2p4): mounted filesystem with ordered data mode. Opts: nomblk_io_submit
init: [libfs_mgr]__mount(source=/dev/block/by-name/cache,target=/cache,type=ext4)=0
init: [libfs_mgr]superblock s_max_mnt_count:10,/dev/block/by-name/vendor
init: [libfs_mgr]Requested quota status is match on /dev/block/by-name/vendor
EXT4-fs (mmcblk2p9): mounted filesystem with ordered data mode. Opts: barrier=1
file system registered
using random self ethernet address
using random host ethernet address
logd.auditd: start
logd.klogd: 25870412002
zram0: detected capacity change from 0 to 314572800
Adding 307196k swap on /dev/block/zram0. Priority:-1 extents:1 across:307196k SS
binder: 263:263 ioctl 620a c424f9ce returned -22
logd.daemon: reinit
rfkill: BT RF going to : off
type=1400 audit(1122.450:4): avc: granted { read } for pid=1 comm="init" name="ttymxc0" dev="tmpfs" ino=10674 scontext=u:r:init:s0 tcontext=u:object_r:tty_device:s0 tclass=chr_file
healthd: unable to get HAL interface, using defaults
healthd: No battery devices found
healthd: battery l=100 v=0 t=42.4 h=2 st=2 chg=a
type=1400 audit(1122.450:4): avc: granted { read } for pid=1 comm="init" name="ttymxc0" dev="tmpfs" ino=10674 scontext=u:r:init:s0 tcontext=u:object_r:tty_device:s0 tclass=chr_file
type=1400 audit(1122.450:5): avc: granted { read open } for pid=1 comm="init" path="/dev/ttymxc0" dev="tmpfs" ino=10674 scontext=u:r:init:s0 tcontext=u:object_r:tty_device:s0 tclass=chr_file
type=1400 audit(1122.450:5): avc: granted { read open } for pid=1 comm="init" path="/dev/ttymxc0" dev="tmpfs" ino=10674 scontext=u:r:init:s0 tcontext=u:object_r:tty_device:s0 tclass=chr_file
type=1400 audit(1122.460:6): avc: granted { read } for pid=307 comm="init" name="ttymxc0" dev="tmpfs" ino=10674 scontext=u:r:init:s0 tcontext=u:object_r:tty_device:s0 tclass=chr_file
type=1400 audit(1122.460:6): avc: granted { read } for pid=307 comm="init" name="ttymxc0" dev="tmpfs" ino=10674 scontext=u:r:init:s0 tcontext=u:object_r:tty_device:s0 tclass=chr_file
type=1400 audit(1122.460:7): avc: granted { read open } for pid=307 comm="init" path="/dev/ttymxc0" dev="tmpfs" ino=10674 scontext=u:r:init:s0 tcontext=u:object_r:tty_device:s0 tclass=chr_file
ERROR: v4l2 capture: slave not found!
ERROR: v4l2 capture: slave not found!
read descriptors
read strings
sabresd_6dq:/ $ android_work: sent uevent USB_STATE=CONNECTED
android_work: sent uevent USB_STATE=DISCONNECTED
android_work: sent uevent USB_STATE=CONNECTED
healthd: battery l=100 v=0 t=42.4 h=2 st=2 chg=a
imx-hdmi-audio imx-hdmi-audio: HDMI Video is not ready!
imx-hdmi-audio imx-hdmi-audio: ASoC: can't open platform imx-hdmi-audio: -22
imx-hdmi-audio imx-hdmi-audio: HDMI Video is not ready!
imx-hdmi-audio imx-hdmi-audio: ASoC: can't open platform imx-hdmi-audio: -22
init: starting service 'bootanim'...
random: crng init done
capability: warning: `main' uses 32-bit capabilities (legacy support in use)
init: processing action (sys.interactive=active) from (/init.freescale.rc:172)
period 0 ,timeout is 0, wake up is :smileylaugh:
period 0 ,timeout is 0, wake up is :smileylaugh:
healthd: battery l=100 v=0 t=42.4 h=2 st=2 chg=a
init: processing action (sys.sysctl.extra_free_kbytes=*) from (/init.rc:682)
init: Unable to open '/proc/sys/vm/extra_free_kbytes': No such file or directory
acc_open
acc_release
Generic PHY 2188000.ethernet:01: attached PHY driver [Generic PHY] (mii_bus:phy_addr=2188000.ethernet:01, irq=-1)
IPv6: ADDRCONF(NETDEV_UP): eth0: link is not ready
selinux: avc: denied { set } for property=persist.netd.stable_secret pid=281 uid=0 gid=0 scontext=u:r:netd:s0 tcontext=u:object_r:default_prop:s0 tclass=property_service permissive=0

init: sys_prop(PROP_MSG_SETPROP2): permission denied uid:0 name:persist.netd.stable_secret
IPv6: ADDRCONF(NETDEV_UP): eth0: link is not ready
init: starting service 'webview_zygote32'...
init: Created socket '/dev/socket/webview_zygote', mode 660, user 1053, group 1000
sdcardfs version 2.0
sdcardfs: dev_name -> /data/media
sdcardfs: options -> fsuid=1023,fsgid=1023,multiuser,mask=6,userid=0,gid=1015
sdcardfs: mnt -> d451b310
sdcardfs: mounted on top of /data/media type ext4
Remount options were mask=23,gid=9997 for vfsmnt d8a7d110.
sdcardfs : options - debug:1
sdcardfs : options - gid:9997
sdcardfs : options - mask:23
Remount options were mask=7,gid=9997 for vfsmnt d461b310.
sdcardfs : options - debug:1
sdcardfs : options - gid:9997
sdcardfs : options - mask:7
alloc_contig_range: [31700, 31eea) PFNs busy
alloc_contig_range: [31800, 31fea) PFNs busy
alloc_contig_range: [31900, 320ea) PFNs busy
type=1400 audit(1124.550:8): avc: denied { read } for pid=301 comm="surfaceflinger" name="dri" dev="tmpfs" ino=10632 scontext=u:r:surfaceflinger:s0 tcontext=u:object_r:device:s0 tclass=dir permissive=0
type=1400 audit(1148.360:9): avc: denied { write } for pid=412 comm="Binder:412_1" name="timerslack_ns" dev="proc" ino=14043 scontext=u:r:system_server:s0 tcontext=u:r:untrusted_app_25:s0:c512,c768 tclass=file permissive=0
type=1400 audit(1148.360:9): avc: denied { write } for pid=412 comm="Binder:412_1" name="timerslack_ns" dev="proc" ino=14043 scontext=u:r:system_server:s0 tcontext=u:r:untrusted_app_25:s0:c512,c768 tclass=file permissive=0
type=1400 audit(1148.360:10): avc: denied { write } for pid=412 comm="Binder:412_1" name="timerslack_ns" dev="proc" ino=15910 scontext=u:r:system_server:s0 tcontext=u:r:untrusted_app_25:s0:c512,c768 tclass=file permissive=0
type=1400 audit(1148.360:10): avc: denied { write } for pid=412 comm="Binder:412_1" name="timerslack_ns" dev="proc" ino=15910 scontext=u:r:system_server:s0 tcontext=u:r:untrusted_app_25:s0:c512,c768 tclass=file permissive=0
type=1400 audit(1148.370:11): avc: denied { write } for pid=412 comm="Binder:412_1" name="timerslack_ns" dev="proc" ino=15912 scontext=u:r:system_server:s0 tcontext=u:r:untrusted_app_25:s0:c512,c768 tclass=file permissive=0
type=1400 audit(1148.370:11): avc: denied { write } for pid=412 comm="Binder:412_1" name="timerslack_ns" dev="proc" ino=15912 scontext=u:r:system_server:s0 tcontext=u:r:untrusted_app_25:s0:c512,c768 tclass=file permissive=0
type=1400 audit(1148.370:12): avc: denied { write } for pid=412 comm="Binder:412_1" name="timerslack_ns" dev="proc" ino=15914 scontext=u:r:system_server:s0 tcontext=u:r:untrusted_app_25:s0:c512,c768 tclass=file permissive=0
type=1400 audit(1148.370:12): avc: denied { write } for pid=412 comm="Binder:412_1" name="timerslack_ns" dev="proc" ino=15914 scontext=u:r:system_server:s0 tcontext=u:r:untrusted_app_25:s0:c512,c768 tclass=file permissive=0
type=1400 audit(1148.370:13): avc: denied { write } for pid=412 comm="Binder:412_1" name="timerslack_ns" dev="proc" ino=15916 scontext=u:r:system_server:s0 tcontext=u:r:untrusted_app_25:s0:c512,c768 tclass=file permissive=0
alloc_contig_range: [31700, 31eea) PFNs busy
alloc_contig_range: [31800, 31fea) PFNs busy
alloc_contig_range: [31900, 320ea) PFNs busy
alloc_contig_range: [33200, 33a74) PFNs busy
alloc_contig_range: [33300, 33b74) PFNs busy
alloc_contig_range: [31700, 31eea) PFNs busy
alloc_contig_range: [31800, 31fea) PFNs busy
alloc_contig_range: [31900, 320ea) PFNs busy
alloc_contig_range: [31a00, 321ea) PFNs busy
alloc_contig_range: [31a00, 322ea) PFNs busy
alloc_contig_range: [31c00, 323ea) PFNs busy
alloc_contig_range: [31c00, 324ea) PFNs busy
alloc_contig_range: [31c00, 325ea) PFNs busy
alloc_contig_range: [31c00, 326ea) PFNs busy
alloc_contig_range: [32000, 327ea) PFNs busy
alloc_contig_range: [32100, 328ea) PFNs busy
alloc_contig_range: [32200, 329ea) PFNs busy
alloc_contig_range: [32300, 32aea) PFNs busy
alloc_contig_range: [32400, 32bea) PFNs busy
alloc_contig_range: [32400, 32cea) PFNs busy
alloc_contig_range: [32600, 32dea) PFNs busy
alloc_contig_range: [32700, 32eea) PFNs busy
alloc_contig_range: [32800, 32fea) PFNs busy
alloc_contig_range: [32900, 330ea) PFNs busy
alloc_contig_range: [31700, 31eea) PFNs busy
alloc_contig_range: [31800, 31fea) PFNs busy
alloc_contig_range: [31900, 320ea) PFNs busy
alloc_contig_range: [31a00, 321ea) PFNs busy
alloc_contig_range: [31a00, 322ea) PFNs busy
alloc_contig_range: [31c00, 323ea) PFNs busy
alloc_contig_range: [31c00, 324ea) PFNs busy
alloc_contig_range: [31c00, 325ea) PFNs busy
alloc_contig_range: [31c00, 326ea) PFNs busy
alloc_contig_range: [32000, 327ea) PFNs busy
alloc_contig_range: [32100, 328ea) PFNs busy
alloc_contig_range: [32200, 329ea) PFNs busy
alloc_contig_range: [33200, 339ea) PFNs busy
alloc_contig_range: [33200, 33aea) PFNs busy
alloc_contig_range: [33400, 33bea) PFNs busy
alloc_contig_range: [31700, 31f74) PFNs busy
alloc_contig_range: [31800, 32074) PFNs busy
alloc_contig_range: [31900, 32174) PFNs busy
alloc_contig_range: [31a00, 32274) PFNs busy
alloc_contig_range: [31a00, 32374) PFNs busy
alloc_contig_range: [31c00, 32474) PFNs busy
alloc_contig_range: [31c00, 32574) PFNs busy
alloc_contig_range: [31c00, 32674) PFNs busy
alloc_contig_range: [31c00, 32774) PFNs busy
alloc_contig_range: [32000, 32874) PFNs busy
alloc_contig_range: [32100, 32974) PFNs busy
period 66 ,timeout is 0, wake up is :smileylaugh:
mma enable setting active
alloc_contig_range: [31700, 31eea) PFNs busy
alloc_contig_range: [31800, 31fea) PFNs busy
alloc_contig_range: [31900, 320ea) PFNs busy
alloc_contig_range: [31a00, 321ea) PFNs busy
alloc_contig_range: [31a00, 322ea) PFNs busy
alloc_contig_range: [31c00, 323ea) PFNs busy
alloc_contig_range: [31c00, 324ea) PFNs busy
alloc_contig_range: [31c00, 325ea) PFNs busy
alloc_contig_range: [31c00, 326ea) PFNs busy
alloc_contig_range: [32000, 327ea) PFNs busy
alloc_contig_range: [32100, 328ea) PFNs busy
alloc_contig_range: [32200, 329ea) PFNs busy
alloc_contig_range: [31700, 31eea) PFNs busy
alloc_contig_range: [31800, 31fea) PFNs busy
alloc_contig_range: [31900, 320ea) PFNs busy
alloc_contig_range: [31a00, 321ea) PFNs busy
alloc_contig_range: [31a00, 322ea) PFNs busy
alloc_contig_range: [31c00, 323ea) PFNs busy
alloc_contig_range: [31c00, 324ea) PFNs busy
alloc_contig_range: [31c00, 325ea) PFNs busy
alloc_contig_range: [31c00, 326ea) PFNs busy
alloc_contig_range: [32000, 327ea) PFNs busy
alloc_contig_range: [32100, 328ea) PFNs busy
alloc_contig_range: [32200, 329ea) PFNs busy
alloc_contig_range: [31700, 31f74) PFNs busy
alloc_contig_range: [31800, 32074) PFNs busy
alloc_contig_range: [31900, 32174) PFNs busy
alloc_contig_range: [31a00, 32274) PFNs busy
alloc_contig_range: [31a00, 32374) PFNs busy
alloc_contig_range: [31c00, 32474) PFNs busy
alloc_contig_range: [31c00, 32574) PFNs busy
alloc_contig_range: [31c00, 32674) PFNs busy
alloc_contig_range: [31c00, 32774) PFNs busy
alloc_contig_range: [32000, 32874) PFNs busy
alloc_contig_range: [32100, 32974) PFNs busy
alloc_contig_range: [31700, 31ed0) PFNs busy
alloc_contig_range: [31800, 31fd0) PFNs busy
alloc_contig_range: [31900, 320d0) PFNs busy
alloc_contig_range: [31a00, 321d0) PFNs busy
alloc_contig_range: [31a00, 322d0) PFNs busy
alloc_contig_range: [31c00, 323d0) PFNs busy
alloc_contig_range: [31c00, 324d0) PFNs busy
alloc_contig_range: [31c00, 325d0) PFNs busy
alloc_contig_range: [31c00, 326d0) PFNs busy
alloc_contig_range: [32000, 327d0) PFNs busy
alloc_contig_range: [32100, 328d0) PFNs busy
alloc_contig_range: [32200, 329d0) PFNs busy
alloc_contig_range: [31700, 31eea) PFNs busy
alloc_contig_range: [31800, 31fea) PFNs busy
alloc_contig_range: [31900, 320ea) PFNs busy
alloc_contig_range: [31a00, 321ea) PFNs busy
alloc_contig_range: [31a00, 322ea) PFNs busy
alloc_contig_range: [31c00, 323ea) PFNs busy
alloc_contig_range: [31c00, 324ea) PFNs busy
alloc_contig_range: [31c00, 325ea) PFNs busy
alloc_contig_range: [31c00, 326ea) PFNs busy
alloc_contig_range: [32000, 327ea) PFNs busy
alloc_contig_range: [32100, 328ea) PFNs busy
alloc_contig_range: [32200, 329ea) PFNs busy
alloc_contig_range: [31700, 32061) PFNs busy
alloc_contig_range: [31800, 32161) PFNs busy
alloc_contig_range: [31900, 32261) PFNs busy
alloc_contig_range: [31a00, 32361) PFNs busy
alloc_contig_range: [31a00, 32461) PFNs busy
alloc_contig_range: [31c00, 32561) PFNs busy
alloc_contig_range: [31c00, 32661) PFNs busy
alloc_contig_range: [31c00, 32761) PFNs busy
alloc_contig_range: [31c00, 32861) PFNs busy
alloc_contig_range: [32000, 32961) PFNs busy
alloc_contig_range: [31700, 32061) PFNs busy
alloc_contig_range: [31800, 32161) PFNs busy
alloc_contig_range: [31900, 32261) PFNs busy
alloc_contig_range: [31a00, 32361) PFNs busy
alloc_contig_range: [31a00, 32461) PFNs busy
alloc_contig_range: [31c00, 32561) PFNs busy
alloc_contig_range: [31c00, 32661) PFNs busy
alloc_contig_range: [31c00, 32761) PFNs busy
alloc_contig_range: [31c00, 32861) PFNs busy
alloc_contig_range: [32000, 32961) PFNs busy
alloc_contig_range: [31700, 32064) PFNs busy
alloc_contig_range: [31800, 32164) PFNs busy
alloc_contig_range: [31900, 32264) PFNs busy
alloc_contig_range: [31a00, 32364) PFNs busy
alloc_contig_range: [31a00, 32464) PFNs busy
alloc_contig_range: [31c00, 32564) PFNs busy
alloc_contig_range: [31c00, 32664) PFNs busy
alloc_contig_range: [31c00, 32764) PFNs busy
alloc_contig_range: [31c00, 32864) PFNs busy
alloc_contig_range: [32000, 32964) PFNs busy
alloc_contig_range: [31700, 31ed0) PFNs busy
alloc_contig_range: [31800, 31fd0) PFNs busy
alloc_contig_range: [31900, 320d0) PFNs busy
alloc_contig_range: [31a00, 321d0) PFNs busy
alloc_contig_range: [31a00, 322d0) PFNs busy
alloc_contig_range: [31c00, 323d0) PFNs busy
alloc_contig_range: [31c00, 324d0) PFNs busy
alloc_contig_range: [31c00, 325d0) PFNs busy
alloc_contig_range: [31c00, 326d0) PFNs busy
alloc_contig_range: [32000, 327d0) PFNs busy
alloc_contig_range: [32100, 328d0) PFNs busy
alloc_contig_range: [32200, 329d0) PFNs busy
init: Service 'bootanim' (pid 403) exited with status 0
init: processing action (sys.boot_completed=1) from (/init.rc:676)
init: processing action (sys.boot_completed=1) from (/init.freescale.rc:164)
init: processing action (sys.boot_completed=1 && sys.logbootcomplete=1) from (/system/etc/init/bootstat.rc:34)
init: starting service 'exec 3 (/system/bin/bootstat --record_boot_complete)'...
init: SVC_EXEC pid 863 (uid 0 gid 0+0 context default) started; waiting...
init: Service 'exec 3 (/system/bin/bootstat --record_boot_complete)' (pid 863) exited with status 0 waiting took 0.083015 seconds
init: starting service 'exec 4 (/system/bin/bootstat --record_boot_reason)'...
init: SVC_EXEC pid 864 (uid 0 gid 0+0 context default) started; waiting...
\0\0

U-Boot 2017.03 (Jan 20 2018 - 10:42:40 +0800)

CPU: Freescale i.MX6Q rev1.2 996 MHz (running at 792 MHz)
CPU: Automotive temperature grade (-40C to 125C) at 44C
Reset cause: POR
Model: Freescale i.MX6 Quad SABRE Smart Device Board
Board: MX6-SabreSD
DRAM: 1 GiB
PMIC: PFUZE100! DEV_ID=0x10 REV_ID=0x21
MMC: FSL_SDHC: 0, FSL_SDHC: 1, FSL_SDHC: 2
No panel detected: default to Hannstar-XGA
Display: Hannstar-XGA (1024x768)
In: serial
Out: serial
Err: serial
flash target is MMC:1
Net: eth0: ethernet@02188000 [PRIME]
Fastboot: Normal
Hit any key to stop autoboot: 3  2  1

Labels (1)
0 Kudos
Reply
1 Solution
2,225 Views
diegoadrian
NXP Employee
NXP Employee

Hello,

Unfortunately, 1GB is not enough memory for Android Oreo. With 2GB could work. But with 4GB will be the best. I apologize for the inconveniences this could give you.

Best Regards,

Diego.

View solution in original post

0 Kudos
Reply
3 Replies
2,225 Views
diegoadrian
NXP Employee
NXP Employee

Hello,

Can you please try using the below bootargs?

U-Boot > setenv bootargs console=ttymxc0,115200 androidboot.console=ttymxc0 consoleblank=0
vmalloc=128M init=/init video=mxcfb0:dev=hdmi,1920x1080M@60,bpp=32 video=mxcfb1:off
video=mxcfb2:off video=mxcfb3:off androidboot.hardware=freescale cma=448M
galcore.contiguousSize=33554432 androidboot.selinux=permissive
U-Boot > saveenv

I have tested those bootargs, and it didn't make the auto reboot as you mentioned. 

Hope this can help you.

Best Regards,

Diego.

0 Kudos
Reply
2,225 Views
lei_zhang1
Contributor I

After that I tried android_N7.1.2_2.0.0_image_6dqpsabresd. The probability of occurrence of the problem is reduced.

But doing things like opening the app, inserting the mouse may still reboot.

Is 1GB RAM too small?

0 Kudos
Reply
2,226 Views
diegoadrian
NXP Employee
NXP Employee

Hello,

Unfortunately, 1GB is not enough memory for Android Oreo. With 2GB could work. But with 4GB will be the best. I apologize for the inconveniences this could give you.

Best Regards,

Diego.

0 Kudos
Reply