imx6 USB_OTG2_PWR in device tree?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

imx6 USB_OTG2_PWR in device tree?

跳至解决方案
5,591 次查看
listplot3d
Contributor III

USB_OTG2_PWR on imx6ul EVK board is pulled to high with hardware.

I have a customer board and need to pull it with software.

I checked below files, but didn't find similar information.

Documentation/devicetree/bindings/usb/fsl-usb.txt

Documentation/devicetree/bindings/usb/generic.txt

Is there any example of how to configure it in device tree?

Thanks & Best Regards

-Shawn

标签 (3)
标记 (1)
0 项奖励
回复
1 解答
3,985 次查看
listplot3d
Contributor III

thanks for all the help.

Below are my settings that made it work.

/arch/arm/boot/dts/imx6ul.dtsi, unchanged

./arch/arm/boot/dts/imx6ul-14x14-evk.dts, modified

aliases {

                gpio0 = &gpio1;

                gpio1 = &gpio2;

                usbphy0 = &usbphy1;

                usbphy1 = &usbphy2;

        };

 

usbphy1: usbphy@020c9000 {

               compatible = "fsl,imx6ul-usbphy", "fsl,imx23-usbphy";

               reg = <0x020c9000 0x1000>;

               interrupts = <GIC_SPI 44 IRQ_TYPE_LEVEL_HIGH>;

               clocks = <&clks IMX6UL_CLK_USBPHY1>;

               phy-3p0-supply = <&reg_3p0>;

               fsl,anatop = <&anatop>;

       };

 

usbmisc: usbmisc@02184800 {

               #index-cells = <1>;

               compatible = "fsl,imx6ul-usbmisc", "fsl,imx6q-usbmisc";

               reg = <0x02184800 0x200>;

};

 

usbotg1: usb@02184000 {

               compatible = "fsl,imx6ul-usb", "fsl,imx27-usb";

               reg = <0x02184000 0x200>;

               interrupts = <GIC_SPI 43 IRQ_TYPE_LEVEL_HIGH>;

               clocks = <&clks IMX6UL_CLK_USBOH3>;

               fsl,usbphy = <&usbphy1>;

               fsl,usbmisc = <&usbmisc 0>;

               fsl,anatop = <&anatop>;

               ahb-burst-config = <0x0>;

               tx-burst-size-dword = <0x10>;

               rx-burst-size-dword = <0x10>;

               status = "disabled";

};

&iomuxc {

...

                  pinctrl_usb_otg1: usbotg1grp {

                                    fsl,pins = <

                                    MX6UL_PAD_GPIO1_IO02__GPIO1_IO02        0x10b0

                                    >;

                  };

};

 

regulators {

                  reg_usb_otg1_vbus: regulator@3 {

                                    compatible = "regulator-fixed";

                                    reg = <3>;

                                    pinctrl-names = "default";

                                    pinctrl-0 = <&pinctrl_usb_otg1>;

                                    regulator-name = "usb_otg1_vbus";

                                    regulator-min-microvolt = <3300000>;

                                    regulator-max-microvolt = <3300000>;

                                    gpio = <&gpio1 2 GPIO_ACTIVE_HIGH>;

                                    regulator-always-on;

                                    enable-active-high;

                  };

};

 

&usbphy1 {

        tx-d-cal = <0x5>;

};

 

&usbotg1 {

                  dr_mode = "host";

                  vbus-supply = <&reg_usb_otg1_vbus>;

                  pinctrl-names = "default";

                  srp-disable;

                  hnp-disable;

                  adp-disable;

                  status = "okay";

};

 

also, delete the imx6ul-14x14-usb-certi.dtd in Boot section.

在原帖中查看解决方案

4 回复数
3,986 次查看
listplot3d
Contributor III

thanks for all the help.

Below are my settings that made it work.

/arch/arm/boot/dts/imx6ul.dtsi, unchanged

./arch/arm/boot/dts/imx6ul-14x14-evk.dts, modified

aliases {

                gpio0 = &gpio1;

                gpio1 = &gpio2;

                usbphy0 = &usbphy1;

                usbphy1 = &usbphy2;

        };

 

usbphy1: usbphy@020c9000 {

               compatible = "fsl,imx6ul-usbphy", "fsl,imx23-usbphy";

               reg = <0x020c9000 0x1000>;

               interrupts = <GIC_SPI 44 IRQ_TYPE_LEVEL_HIGH>;

               clocks = <&clks IMX6UL_CLK_USBPHY1>;

               phy-3p0-supply = <&reg_3p0>;

               fsl,anatop = <&anatop>;

       };

 

usbmisc: usbmisc@02184800 {

               #index-cells = <1>;

               compatible = "fsl,imx6ul-usbmisc", "fsl,imx6q-usbmisc";

               reg = <0x02184800 0x200>;

};

 

usbotg1: usb@02184000 {

               compatible = "fsl,imx6ul-usb", "fsl,imx27-usb";

               reg = <0x02184000 0x200>;

               interrupts = <GIC_SPI 43 IRQ_TYPE_LEVEL_HIGH>;

               clocks = <&clks IMX6UL_CLK_USBOH3>;

               fsl,usbphy = <&usbphy1>;

               fsl,usbmisc = <&usbmisc 0>;

               fsl,anatop = <&anatop>;

               ahb-burst-config = <0x0>;

               tx-burst-size-dword = <0x10>;

               rx-burst-size-dword = <0x10>;

               status = "disabled";

};

&iomuxc {

...

                  pinctrl_usb_otg1: usbotg1grp {

                                    fsl,pins = <

                                    MX6UL_PAD_GPIO1_IO02__GPIO1_IO02        0x10b0

                                    >;

                  };

};

 

regulators {

                  reg_usb_otg1_vbus: regulator@3 {

                                    compatible = "regulator-fixed";

                                    reg = <3>;

                                    pinctrl-names = "default";

                                    pinctrl-0 = <&pinctrl_usb_otg1>;

                                    regulator-name = "usb_otg1_vbus";

                                    regulator-min-microvolt = <3300000>;

                                    regulator-max-microvolt = <3300000>;

                                    gpio = <&gpio1 2 GPIO_ACTIVE_HIGH>;

                                    regulator-always-on;

                                    enable-active-high;

                  };

};

 

&usbphy1 {

        tx-d-cal = <0x5>;

};

 

&usbotg1 {

                  dr_mode = "host";

                  vbus-supply = <&reg_usb_otg1_vbus>;

                  pinctrl-names = "default";

                  srp-disable;

                  hnp-disable;

                  adp-disable;

                  status = "okay";

};

 

also, delete the imx6ul-14x14-usb-certi.dtd in Boot section.

3,985 次查看
weidong_sun
NXP TechSupport
NXP TechSupport

Hello Li,

    USB_OTG2_PWR net on schematic is connected to GPIO_2 of I.MX6UL, But this pin is not used, see schematic:

pastedImage_1.png

But DCDC_3V3 is used to enable USB OTG2 Power. So GPIO_2 pin doesn't need to be handled in device treee.

In addition, you should read these documents :

(1) i.MX6UltraLite Evaluation Kit|NXP 

(2) Reading Linux BSP for i.MX6UL evaluation board.

 Have a nice day!

Best Regards,

Weidong

0 项奖励
回复
3,985 次查看
listplot3d
Contributor III

Hi weidong.sun,

   Thanks for your reply. I knew the place of schematics about EVK you mentioned, and my question was, with schematics below, how to config device tree?

Thanks & Regards

-Shawn

Capture1.PNG

Capture.PNG

0 项奖励
回复
3,985 次查看
tengri
Contributor IV

Hi, in your dts or dtsi file you can specify it as follows (in my example I am using a different GPIO for that) :

pinctrl_reg_usbotg_vbus: reg-usbotg-vbusgrp {
         fsl,pins = <
#define OTG_POWER <&gpio3 22 GPIO_ACTIVE_HIGH>
                  MX6QDL_PAD_EIM_D22__GPIO3_IO22 0x030b0
         >;
};

The bold color term is the default functionality of the the pin GPIO3_IO22, you can find the correct definition for your pin in pin_function.h file.

Anuradha

0 项奖励
回复