imx6 ONOFF button can make a interrupt to arm core.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

imx6 ONOFF button can make a interrupt to arm core.

跳至解决方案
4,096 次查看
chuanyanyin
Contributor III

Hi, ChipExpert:

  I Have a custom board, the OnOff button can control pmic_on_req when I press the button more than 5 seconds. 

According the mx6's manual,  10.5 on page 545.

• When the chip main power supply is On, a button press between 750 ms and 5

seconds will send an interrupt to the core to request that software bring down the

SoC safely. Software may respond to the interrupt by saving the processor state and

then setting a control bit that requests to the power IC the removal of the main power

supply.

When I shorten OnOff and GND more than 750 ms, I don't see any things happened in the kernel's log.

How can I make this interrupt happened? I don't find any source code in linux3.0.35 and android 4.3.

标签 (4)
0 项奖励
回复
1 解答
2,348 次查看
igorpadykov
NXP Employee
NXP Employee

Hi chuanyan

I believe links below answer this

ONOFF button doesn't interrupt

ARM: i.MX6: SNVS ONOFF: Add SNVS Power key support - Gitorious

Best regards

chip

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
2 回复数
2,349 次查看
igorpadykov
NXP Employee
NXP Employee

Hi chuanyan

I believe links below answer this

ONOFF button doesn't interrupt

ARM: i.MX6: SNVS ONOFF: Add SNVS Power key support - Gitorious

Best regards

chip

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复
2,348 次查看
lytkinanton
Contributor I

Hi,

Pls, give some advice for next situation:

I use snvs power key patch. Interrupts are present when system is active. When I do "apm -s", there is no interrupts from snvs_pwrkey and no system wakeup. When I wake system by other source (uart in my case), interrupts "snvs_pwrkey" appears again.

What I'm doing wrong?

PS: Can we speak Russian at this forum?

0 项奖励
回复