imx28 boot failure (0x80501003) after reflashing

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx28 boot failure (0x80501003) after reflashing

2,815 Views
jordifarres
Contributor III

Hi,

My system boots from a serial flash spi and works fine. But after a reflashing process it always fail when reseting.

The error code reported is 0x80501003 and de booting process is halted.

Next reset goes fine.

Does anyone know what can be happening ?

thanks

jordi

0 Kudos
Reply
5 Replies

2,115 Views
YixingKong
Senior Contributor IV

Jordi

We have not got your response yet and will close the discussion in 3 days. If you still need help, please feel free to reply with an update to this discussion.

Thanks,

Yixing

0 Kudos
Reply

2,115 Views
YixingKong
Senior Contributor IV

Jordi

Had your issue got resolved? If yes, we are going to close the discussion in 3 days. If you still need help, please feel free to reply with an update to this discussion.

Thanks,

Yixing

0 Kudos
Reply

2,115 Views
alejandrolozan1
NXP Employee
NXP Employee

Hi,

Does it only happen after reflashing the SPI flash?

I checked ant the error code is this : 0x80501003 The file signature or file version is incorrect.

Are you using HAB? Can you give more details?

Best Regards,

Alejandro

0 Kudos
Reply

2,115 Views
bruce_chen
Contributor I

Hi Alejandrolozano:

     I am using HAB for imx28, but now using Mfgtool Programming updater_ivt.sb and imx28_ivt_linux.sb, The serial port output 0x80501001 DCP Error Code, I don't know how making the HAB SB files. My operation step according to AN4555.pdf. thanks.

0 Kudos
Reply

2,115 Views
jordifarres
Contributor III

Hi Alejandro

I am not using HAB.

It only happens after reflashing. Not always but in the most cases.

This happens regardless of using MfgTool, u-boot or from a linux application to reflash.

The effect occurs both my board design as EVK.

When the system gets stuck, showing 0x80501003 code, it remains in this state indefinitely and only gets out with a new reset pulse.

In this state ROM doesn't retry to boot, and would be better do that.

If I make a reboot command after reflashing then never fails.

regards

jordi

0 Kudos
Reply