hi,
1:what is the ic of 4cvbs_camera in for imx6q in FSL's demo,also support for driver?
Is it tw2866 or te2867?or others.Please give me some links or files for 4-cvbs_camera input for imx6q demo.
Thanks.
Hi
please look at below link with example driver for Maxim MAX9286, it was verified working
on iMX6DQ SabreAuto board. The input to MAX9286 is four 720P30 cameras.
Also verified camera boards:
(1) Onsemi AR0140+AP0101+MAX9271 boards.
(2) OmniVision OV10635+MAX9271 boards.
https://community.freescale.com/docs/DOC-328548
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
hi,
Thanks.
1:I prefer to use csi0 to connect 4_cvbs_camera in. So the same question.