imx28 LTIB RPMs not found anymore?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

imx28 LTIB RPMs not found anymore?

2,747件の閲覧回数
jannyman
Contributor II

Hi all,

I am attempting to build an image for imx2833 using LTIB  (from L2.6.35_1.1.0_130130_source.tar.gz). However, it seems that some of the RPMs are no longer accessible.

After "Testing network connectivity" it returns "OK GPP", but when it attempts to download the Linaro gcc RPM from bitshrine.org, a 404 error is returned.

Please see the attached screenshot for details.

Is there a mirror for the files, and how do I configure it to use a mirror instead?

BR,

Jan

タグ(1)
0 件の賞賛
返信
1 返信

2,673件の閲覧回数
gusarambula
NXP TechSupport
NXP TechSupport

Hello Jay Nyman,

This is a common problem since the BSP was released quite a while ago. Please try with the suggestions on the following thread and let us know if that helps.

Can't get: gcc-4.6.2-glibc-2.13-linaro-multilib-2011.12-1.i386.rpm at ./ltib line 2560.

0 件の賞賛
返信