imx258: address of pu_irom_error_status (HAB status)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx258: address of pu_irom_error_status (HAB status)

890 Views
martinskaiser
Contributor I

Dear all,

the imx258 specifications list two different values for the address where the HAB status is stored. The reference manual claims that the address is 0x780018C0 and the security reference manual says that the status is at 0x780018D4.

It seems to me that the latter address is the correct one. Can anyone confirm this?

Thanks,

Martin

Labels (1)
0 Kudos
Reply
1 Reply

797 Views
igorpadykov
NXP Employee
NXP Employee

Hi Martin

you are right, latter address is the correct.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply