imx258: address of pu_irom_error_status (HAB status)

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

imx258: address of pu_irom_error_status (HAB status)

894件の閲覧回数
martinskaiser
Contributor I

Dear all,

the imx258 specifications list two different values for the address where the HAB status is stored. The reference manual claims that the address is 0x780018C0 and the security reference manual says that the status is at 0x780018D4.

It seems to me that the latter address is the correct one. Can anyone confirm this?

Thanks,

Martin

ラベル(1)
0 件の賞賛
返信
1 返信

801件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Martin

you are right, latter address is the correct.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信