imx-weim

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

imx-weim

2,591件の閲覧回数
niklasmolin
Senior Contributor I

Hi.

I'm wonder if someone has an example how to use the imx-weim driver?

Thanks,

Niklas

ラベル(2)
0 件の賞賛
返信
1 返信

1,899件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Niklas

"weim" is usually supported through parallel NOR flash driver,

which present in i.MX Auto boards, for example below i.MX6 Sabre Auto

links. i.MX_6Dual6Quad_Linux_Reference_Manual.pdf describes weim nor driver.

L3.0.35_4.1.0_LINUX_DOCS

RDIMX6SABREAUTO: SABRE for Automotive Infotainment Based on the i.MX 6 Series: SABRE for Automotive ...

Best regards

chip

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信