imx-ipuv3 imx-ipuv3.0: DC stop timeout - 0 * 10ms

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

imx-ipuv3 imx-ipuv3.0: DC stop timeout - 0 * 10ms

ソリューションへジャンプ
1,455件の閲覧回数
pfsang
Contributor IV

hi, all

     i  encountered a problem about ipu.

     i'm porting linux on imx6 customized board.

     after power-on , it can display the linux log on lvds panel. it also can play video with gstreamer.

     but after several minutes, it displays nothing and just becomes Black-screen.

     it will show the following message on the console

-------------------------------------------------------------------------------

     imx-ipuv3 imx-ipuv3.0: DC stop timeout - 0 * 10ms

     mxc_ldb mxc_ldb: LDB blank, control reg:0x200

--------------------------------------------------------------------------------

     what's problem with it.?

ラベル(5)
0 件の賞賛
返信
1 解決策
1,186件の閲覧回数
qiang_li-mpu_se
NXP Employee
NXP Employee

It is linux timeout to blank screen, you can add "consoleblank=0" in your boot command to avoid such timeout.

元の投稿で解決策を見る

0 件の賞賛
返信
4 返答(返信)
1,187件の閲覧回数
qiang_li-mpu_se
NXP Employee
NXP Employee

It is linux timeout to blank screen, you can add "consoleblank=0" in your boot command to avoid such timeout.

0 件の賞賛
返信
1,186件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi fang

"control reg:0x200" means that LDB was reset

and stopped (disabled). Many reasons may cause it:

DDR errors, power supply issues, just errors in software.

I would suggest to start with hardware and check LDB

with SDK (one can run it with jtag)

i.MX 6Series Platform SDK : Bare-metal SDK

Best regards

chip

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
1,186件の閲覧回数
pfsang
Contributor IV

hi, chipexpert

       Does "power supply issues" means that pmic will also cause the error?

      and to i.MX 6Series Platform SDK : Bare-metal SDK ,

       how to test it with it ?

      i found the ips_test.c in iMX6_Platform_SDK\sdk\drivers\ipu\test.

      is this test file?

B&R

peter

0 件の賞賛
返信
1,186件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi fang

yes pmic also can reset LDB.

For SDK, first please read documentation

included in that package,

Then please create (if necessary) new community thread.

Best regards

chip

0 件の賞賛
返信