imx-ipuv3 imx-ipuv3.0: DC stop timeout - 0 * 10ms

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx-ipuv3 imx-ipuv3.0: DC stop timeout - 0 * 10ms

Jump to solution
1,124 Views
pfsang
Contributor IV

hi, all

     i  encountered a problem about ipu.

     i'm porting linux on imx6 customized board.

     after power-on , it can display the linux log on lvds panel. it also can play video with gstreamer.

     but after several minutes, it displays nothing and just becomes Black-screen.

     it will show the following message on the console

-------------------------------------------------------------------------------

     imx-ipuv3 imx-ipuv3.0: DC stop timeout - 0 * 10ms

     mxc_ldb mxc_ldb: LDB blank, control reg:0x200

--------------------------------------------------------------------------------

     what's problem with it.?

Labels (5)
0 Kudos
Reply
1 Solution
855 Views
qiang_li-mpu_se
NXP Employee
NXP Employee

It is linux timeout to blank screen, you can add "consoleblank=0" in your boot command to avoid such timeout.

View solution in original post

0 Kudos
Reply
4 Replies
856 Views
qiang_li-mpu_se
NXP Employee
NXP Employee

It is linux timeout to blank screen, you can add "consoleblank=0" in your boot command to avoid such timeout.

0 Kudos
Reply
855 Views
igorpadykov
NXP Employee
NXP Employee

Hi fang

"control reg:0x200" means that LDB was reset

and stopped (disabled). Many reasons may cause it:

DDR errors, power supply issues, just errors in software.

I would suggest to start with hardware and check LDB

with SDK (one can run it with jtag)

i.MX 6Series Platform SDK : Bare-metal SDK

Best regards

chip

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply
855 Views
pfsang
Contributor IV

hi, chipexpert

       Does "power supply issues" means that pmic will also cause the error?

      and to i.MX 6Series Platform SDK : Bare-metal SDK ,

       how to test it with it ?

      i found the ips_test.c in iMX6_Platform_SDK\sdk\drivers\ipu\test.

      is this test file?

B&R

peter

0 Kudos
Reply
855 Views
igorpadykov
NXP Employee
NXP Employee

Hi fang

yes pmic also can reset LDB.

For SDK, first please read documentation

included in that package,

Then please create (if necessary) new community thread.

Best regards

chip

0 Kudos
Reply