imx-gst1.0-plugin / VPU Encoding firmware Issue for setting the QP in VBR mode

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx-gst1.0-plugin / VPU Encoding firmware Issue for setting the QP in VBR mode

Jump to solution
453 Views
KrishnaraoP
Contributor I

I am using 8M Plus SOM and using imx-gst1.0-plugin in our application for H264 encoding.

There is no API to limit the QP for I frame.

We decided to use VBR hence set the bitrate as zero i.e. enc->open_param.nBitRate = 0.

After that setting the QP for I frame as 35 and for Pframe as 25 through enc_enc_param.nQuantParam.

After encoding, observed QP 35 for I frames and QP 40 for P frames.

As per the manual


bitRate is the target bit rate in kbps. If 0, there is no rate control and pictures are encoded with a quantization parameter equal to quantParam in EncParam.


quantParam is used for all quantization parameters with VBR (no rate control). The range of value is 1-31 for MPEG-4 and 0-51 for H.264. When rate control is enabled, this field is ignored.

Clearly it's a bug in the Plug-in / firmware.

Please look into the issue and provide a solution.

0 Kudos
Reply
1 Solution
231 Views
Tashia
NXP Employee
NXP Employee

Hi @KrishnaraoP 

I wanted to share please if you can use gstreamer pipeline in order to run the encoder on i.MX8MPlus. There is no issue in the VPU firmware and we can control QP for the I and P frames.

 

Few things to consider: talking about QP for I frame, that if frame_level_rate_control is 1, hevc_minimum_qp_value and hevc_maximum_qp_value are used in the pipeline. If frame_level_rate_control is 0 then only hevc_i_frame_qp_value take into effect (or try modifying all the controls).

 

for example: frame_level_rate_control is 0 : v4l2h265enc extra-controls="controls,hevc_profile=1,hevc_level=15,hevc_i_frame_qp_value =20")and check if it works as expected, or modify all the controls to get it working. (qpMin/qpMax and qp in this case -  for example: v4l2h265enc extra-controls="controls,hevc_profile=1,hevc_level=15,hevc_maximum_qp_value=20, hevc_i_frame_qp_value=19")

For V4L2 codec observations:

Tashia_5-1756805606312.png

 

you can list the V4L2 control supported by the device.

root@imx8mpevk:~# v4l2-ctl -d /dev/video0 -l 

Tashia_4-1756801401177.png

i.MX Linux User guide has numerous gstreamer pipeline to get an idea about usage of different plugins. Topic especially related to encoding section 7.3.3 Video encoding page 63.

 

For h265 as an example a gstreamer pipeline, as follows:

gst-launch-1.0 filesrc location=out.nv12 ! rawvideoparse width=3840 height=2160 format=nv12 framerate=30/1 colorimetry=bt709 ! v4l2h264enc extra-controls="controls,h264_profile=1,h264_level=15,h264_minimum_qp_value=20, h264_i_frame_qp_value=22" ! filesink location=qp22_test.h264

 

Moreover, https://community.nxp.com/t5/i-MX-Processors/8M-Plus-H264-Encoding-issues-unreliable-firmware/m-p/21...seems to be the same issue kindly let me know if further information is required. 

Kind Regards,

Tashia

View solution in original post

0 Kudos
Reply
4 Replies
209 Views
KrishnaraoP
Contributor I

Hi

I observed two issues, 

extra-controls="controls,video_bitrate_mode=1,video_bitrate=4000000,video_gop_size=60, slice_partitioning_method=1, number_of_mbs_in_a_slice=17, frame_level_rate_control_enable=1, h264_profile=4, h264_minimum_qp_value=25, h264_maximun_qp_value=45"

 

a) encoding in baseline profile only

b) frame_level_rate_control_enable=1, and h264_minimum_qp_value=25, h264_maximun_qp_value=45 but I observed qp=48 for the first and second frame, third frame qp as 46. 

0 Kudos
Reply
428 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

Please send is you BSP and the whole steps you made to see that VPU does not work.

Regards

0 Kudos
Reply
404 Views
KrishnaraoP
Contributor I

Hi

Linux version 6.6.52-lts-next (aarch64-poky-linux-gcc (GCC) 13.3.0, GNU ld (GNU Binutils) 2.42.0.20240723) #1 SMP PREEMPT 

in imx-gst1.0-plugin i.e. imx-gst1.0-plugin\plugins\vpu\gstvpuenc.c file

a) set the bitrate to zero i.e. in gst_vpu_enc_set_format function

enc->open_param.nBitRate = 0;

b) assigning the quantiztion parameter based on the frametype

in gst_vpu_enc_handle_frame

if (enc_enc_param.nForceIPicture == 1)

    enc_enc_param.nQuantParam  = 35;

else

   enc_enc_param.nQuantParam  = 30;

 

it is not working, no support in imx-vpuwrap package.

 
0 Kudos
Reply
232 Views
Tashia
NXP Employee
NXP Employee

Hi @KrishnaraoP 

I wanted to share please if you can use gstreamer pipeline in order to run the encoder on i.MX8MPlus. There is no issue in the VPU firmware and we can control QP for the I and P frames.

 

Few things to consider: talking about QP for I frame, that if frame_level_rate_control is 1, hevc_minimum_qp_value and hevc_maximum_qp_value are used in the pipeline. If frame_level_rate_control is 0 then only hevc_i_frame_qp_value take into effect (or try modifying all the controls).

 

for example: frame_level_rate_control is 0 : v4l2h265enc extra-controls="controls,hevc_profile=1,hevc_level=15,hevc_i_frame_qp_value =20")and check if it works as expected, or modify all the controls to get it working. (qpMin/qpMax and qp in this case -  for example: v4l2h265enc extra-controls="controls,hevc_profile=1,hevc_level=15,hevc_maximum_qp_value=20, hevc_i_frame_qp_value=19")

For V4L2 codec observations:

Tashia_5-1756805606312.png

 

you can list the V4L2 control supported by the device.

root@imx8mpevk:~# v4l2-ctl -d /dev/video0 -l 

Tashia_4-1756801401177.png

i.MX Linux User guide has numerous gstreamer pipeline to get an idea about usage of different plugins. Topic especially related to encoding section 7.3.3 Video encoding page 63.

 

For h265 as an example a gstreamer pipeline, as follows:

gst-launch-1.0 filesrc location=out.nv12 ! rawvideoparse width=3840 height=2160 format=nv12 framerate=30/1 colorimetry=bt709 ! v4l2h264enc extra-controls="controls,h264_profile=1,h264_level=15,h264_minimum_qp_value=20, h264_i_frame_qp_value=22" ! filesink location=qp22_test.h264

 

Moreover, https://community.nxp.com/t5/i-MX-Processors/8M-Plus-H264-Encoding-issues-unreliable-firmware/m-p/21...seems to be the same issue kindly let me know if further information is required. 

Kind Regards,

Tashia

0 Kudos
Reply