imx-drm framebuffer rotation

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx-drm framebuffer rotation

3,252 Views
ottawa-imx6
Contributor IV

Hello, I am using the imx-drm with a parallel rgb lcd under 3.18. I have it working a little, but there are a few little issues that I am still working on.

1. Does anyone know how to do a permanent 180 degree vertical flip of the framebuffer contents while using imx-drm? I would like this in the kernel upon initialization.

2. Strangely, I had to enable the framebuffer console in my configuration to get the display to work at all... I don't need the fbcon, but there must be something that it does to enable my drm setup to work.

3. While using imx-drm, what do we set our bootargs in u-boot to? Previously, I had reference to mxcfb0, but now that we are using imx-drm, there is no reference to this mxcfb0. This could be the root cause of the above, but I cannot find any documentation on it.

Thanks

Brent

Labels (2)
Tags (1)
0 Kudos
Reply
3 Replies

2,416 Views
fabio_estevam
NXP Employee
NXP Employee

Brent,

Please ask these questions at dri-devel@lists.freedesktop.org mailing list with the imx drm maintainer on Cc: Philipp Zabel <p.zabel@pengutronix.de>.

0 Kudos
Reply

2,416 Views
ottawa-imx6
Contributor IV

Will do, thank you.

Brent

0 Kudos
Reply

2,416 Views
ivannikolaenko
Contributor IV

Hi, Brent.

Did you solve your problem?

We faced it too.

0 Kudos
Reply