imx.6 boot from eMMC (eMMC version )

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

imx.6 boot from eMMC (eMMC version )

1,563 次查看
ravivhaim
Contributor I

Hi,

I've noticed that the imx.6 can boot from eMMC 4.4 or lower.

would it be possible to boot a custom board from eMMC 5.0 or 5.1 ?

Thanks,

Raviv

标签 (1)
0 项奖励
回复
1 回复

1,269 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Raviv

yes possible, boot ROM will fall back to the eMMC4.4 standard

when a eMMC 5.0, 5.1 capable device is detected.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复