imx.6 boot from eMMC (eMMC version )

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx.6 boot from eMMC (eMMC version )

1,629 Views
ravivhaim
Contributor I

Hi,

I've noticed that the imx.6 can boot from eMMC 4.4 or lower.

would it be possible to boot a custom board from eMMC 5.0 or 5.1 ?

Thanks,

Raviv

Labels (1)
0 Kudos
Reply
1 Reply

1,335 Views
igorpadykov
NXP Employee
NXP Employee

Hi Raviv

yes possible, boot ROM will fall back to the eMMC4.4 standard

when a eMMC 5.0, 5.1 capable device is detected.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply