icecast audio streaming on android 5.1 default browser

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

icecast audio streaming on android 5.1 default browser

1,682 次查看
yenchao
Contributor IV

Hi,

I'm working on android 5.1 with imx6dl for playing audio streaming  from a icecast server.

When I enter below url  and click start button by android default browser.

http://202.212.210.163/test/abe_autoplay/audio0511.html

It will show some error messages as follows.

----------------------------------

I/OMXPlayer( 191): Loading content: http://202.212.210.163:8000/ices
I/OMXPlayer( 191): LEVEL: 1 FUNCTION: MediaTypeInspect LINE: 1965
I/OMXPlayer( 191): Can't inspect media content type by subfix.
E/SQLiteLog( 1175): (284) automatic index on sqlite_sq_AF150D80(url)
I/OMXPlayer( 191): LEVEL: 1 FUNCTION: GetContentLength LINE: 115
I/OMXPlayer( 191): GetContentLength url_seek AVSEEK_SIZE fail
PU: Power-off latency exceeded, new value 25667 ns
I/OMXPlayer( 191): transfer_func data timeout.
I/OMXPlayer( 191): LEVEL: 1 FUNCTION: Seek LINE: 277
I/OMXPlayer( 191): HttpsProtocol::Seek() fail, ret -1, request 5120
I/OMXPlayer( 191): server seekable: 1
I/OMXPlayer( 191): HttpsProtocol::Read() terminated
I/OMXPlayer( 191): file size: 0, buffer size : 0

I/OMXPlayer( 191): transfer_func data timeout.
I/OMXPlayer( 191): LEVEL: 1 FUNCTION: GetContentLength LINE: 115
I/OMXPlayer( 191): GetContentLength url_seek AVSEEK_SIZE fail
I/OMXPlayer( 191): server seekable: 0
I/OMXPlayer( 191): transfer_func data timeout.
I/OMXPlayer( 191): LEVEL: 1 FUNCTION: Seek LINE: 277
I/OMXPlayer( 191): HttpsProtocol::Seek() fail, ret -1, request 0
I/OMXPlayer( 191): LEVEL: 1 FUNCTION: GetContentLength LINE: 115
I/OMXPlayer( 191): GetContentLength url_seek AVSEEK_SIZE fail
I/OMXPlayer( 191): LEVEL: 1 FUNCTION: GetContentLength LINE: 115
I/OMXPlayer( 191): GetContentLength url_seek AVSEEK_SIZE fail
I/OMXPlayer( 191): LEVEL: 1 FUNCTION: GetContentLength LINE: 115
I/OMXPlayer( 191): GetContentLength url_seek AVSEEK_SIZE fail
I/OMXPlayer( 191): LEVEL: 1 FUNCTION: GetContentLength LINE: 115
I/OMXPlayer( 191): GetContentLength url_seek AVSEEK_SIZE fail
I/OMXPlayer( 191): LEVEL: 1 FUNCTION: GetContentLength LINE: 115
I/OMXPlayer( 191): GetContentLength url_seek AVSEEK_SIZE fail
I/OMXPlayer( 191): LEVEL: 1 FUNCTION: GetContentLength LINE: 115
I/OMXPlayer( 191): GetContentLength url_seek AVSEEK_SIZE fail
I/OMXPlayer( 191): LEVEL: 1 FUNCTION: GetContentLength LINE: 115
I/OMXPlayer( 191): GetContentLength url_seek AVSEEK_SIZE fail

-----------------------------------------------

If I install and use chrome browser to play this audio streaming then everything goes well.

Does anyone know how to fix this issue?

Any advice and suggestion would be greatly appreicated.

Thx

Yen

标签 (4)
0 项奖励
回复
2 回复数

1,489 次查看
diegoadrian
NXP Employee
NXP Employee

Hello, 

I do not know if you are still having a problem.

If yes, can you please tell me which command are you using to stream the Audio? or, are you using an application?

Best Regards,

Diego.

0 项奖励
回复

1,489 次查看
yenchao
Contributor IV

Hi Diego,

The problem is not solved.

I'm using android 5.1 default browser.

Thx

Yen

0 项奖励
回复