iMx53 VPU&IPU

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
5,670件の閲覧回数
deepanrajanbara
Contributor IV

Hi,

Ours is IMx53 processor,

Is there any Binaries/Firmware dependency to be loaded for VPU and IPU drivers on imx53.

If Binaries or Firmware is required Please share the link.

Thank you,

Deepanraj.A

ラベル(4)
0 件の賞賛
返信
1 解決策
5,355件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Deepanraj

for vpu firmware please refer to attached Linux Manual

Table 18-3. VPU firmware Files. It works with vpu codecs on below links

Board Support Packages (8)

Linux 2.6.35 Source Code Files and documentation 11.09

"Linux Multimedia Codecs Documentation and Sources 11.09 for i.MX53 for the

Codecs and other Algorithms (1)

Quick Start boards.Updated with the Linux 11.09 patch release and the 2.0.5 Open Max files. (REV 2011.09.03)

http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=IMX53QSB&fpsp=1&tab=Design_Tools_Tab

IPU drivers are described in Chapter 10 Image Processing Unit (IPU) Drivers,

regarding dependencies one can check attached Release Notes

Table 1-1,Table 1-2 show used kernel,toolchain versions.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
5,356件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Deepanraj

for vpu firmware please refer to attached Linux Manual

Table 18-3. VPU firmware Files. It works with vpu codecs on below links

Board Support Packages (8)

Linux 2.6.35 Source Code Files and documentation 11.09

"Linux Multimedia Codecs Documentation and Sources 11.09 for i.MX53 for the

Codecs and other Algorithms (1)

Quick Start boards.Updated with the Linux 11.09 patch release and the 2.0.5 Open Max files. (REV 2011.09.03)

http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=IMX53QSB&fpsp=1&tab=Design_Tools_Tab

IPU drivers are described in Chapter 10 Image Processing Unit (IPU) Drivers,

regarding dependencies one can check attached Release Notes

Table 1-1,Table 1-2 show used kernel,toolchain versions.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信