Voltage of USB OTG DP pin of i.MX6

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Voltage of USB OTG DP pin of i.MX6

761 Views
宗標廖
Contributor V

Hello,Community

I have an issue about the voltage of USB OTG DP pin of i.MX6.

In normal case, the DP pin should have a voltage change as bellow when the kernel is starting up.

※I measured it on i.MX6DLSabreAuto and connected the OTG port to PC.

But my customer met an problem. On their board, after the D+ pin rising to 0.6V, it will not fall down

and keep on 0.6V for ever.

Could you give me some advice to analyze the reason?(I think it is something about kernel,but I have not find it)

usb_otg_dp_0_6.png

Best Regards,

ZongbiaoLiao

Labels (2)
0 Kudos
Reply
4 Replies

645 Views
igorpadykov
NXP Employee
NXP Employee

Hi ZongbiaoLiao

main points for check USB_LDO (VDD_VBUS_CAP) voltage,

24MHz signal quality and possibility of ESD damage. It may be useful

to check sect.3.14 i.MX6 System Development User’s Guide (rev.1, 6/2013)

http://cache.freescale.com/files/32bit/doc/user_guide/IMX6DQ6SDLHDG.pdf

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

645 Views
宗標廖
Contributor V

Hi Igor

Please help me!

Thank you very much!

0 Kudos
Reply

645 Views
igorpadykov
NXP Employee
NXP Employee

Hi ZongbiaoLiao

behaviour of usb signals is described in USB 2.0 specificaion

USB.org - Documents

Best regards

igor

0 Kudos
Reply

645 Views
宗標廖
Contributor V

Hi Igor

Thank you for your reply!

In normal case,why does OTG D+ pin have a voltage change as above(why does it need this)?

Please explain the reason.

Best Regards,

ZongbiaoLiao

0 Kudos
Reply