iMXRT1170 Boot from eMMC boot1 partition

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

iMXRT1170 Boot from eMMC boot1 partition

2,300 次查看
yangaichimantou
Contributor I

Hi,

Now We can boot from eMMC User Area partition by MCU BootUtility.

However,when we try to boot from eMMC boot1 partition.

It can not work.

We want to know how to set the configuration of MCU BootUtility or other modification of the system to

let the iMXRT1170 boot from Boot1 partition?

Hope for your reply.

标签 (1)
0 项奖励
回复
4 回复数

1,716 次查看
Greenhal
Contributor II

I have found a way to boot from the eMMC boo1 partition with MIMXRT1170-EVKB. Below you can find the steps to make it work:

  1. Set target setup as follows

    Greenhal_1-1720690431928.png

  2.  Click the “Boot device Configuration” button and set all the fields as presented below
     

     

     Greenhal_3-1720690562284.png

  3.  Set the MiMXRT board in SDP Mode and load the image
  4. Power off the board
  5. Set the boot switches as follows - sw1 "0.0.1.0" sw2 "1.0.0.0.0.0.0.1.0.0"
  6. Power on the board
  7. The software loaded to the eMMC boot 1 partition should start

2,272 次查看
EdwinHz
NXP TechSupport
NXP TechSupport

Hi @yangaichimantou,

Is the issue discussed on the following community post related to what you are experiencing? https://community.nxp.com/t5/i-MX-RT/Boot-loader-behaviour-on-i-MX-RT-1021/m-p/1468975

Also, have you looked into the MCU BootUtility owner's blog? https://www.cnblogs.com/henjay724/

 

BR,

Edwin

0 项奖励
回复

2,266 次查看
yangaichimantou
Contributor I

No, my main problem is not with MCU BootUtility.

I want to boot from eMMC boot1 partition.This is our main problem.

Now we can boot from eMMC user data partition.

0 项奖励
回复

1,787 次查看
Greenhal
Contributor II

Hi,

I also try to boot from eMMC boot1 partition but without success.

Did you resolve the problem? Can you share the solution?

0 项奖励
回复